AM243x MCU+ SDK  08.04.00
mod_null.h
Go to the documentation of this file.
1 /*
2  * Copyright (c) Texas Instruments Incorporated 2020
3  *
4  * Redistribution and use in source and binary forms, with or without
5  * modification, are permitted provided that the following conditions
6  * are met:
7  *
8  * Redistributions of source code must retain the above copyright
9  * notice, this list of conditions and the following disclaimer.
10  *
11  * Redistributions in binary form must reproduce the above copyright
12  * notice, this list of conditions and the following disclaimer in the
13  * documentation and/or other materials provided with the
14  * distribution.
15  *
16  * Neither the name of Texas Instruments Incorporated nor the names of
17  * its contributors may be used to endorse or promote products derived
18  * from this software without specific prior written permission.
19  *
20  * THIS SOFTWARE IS PROVIDED BY THE COPYRIGHT HOLDERS AND CONTRIBUTORS
21  * "AS IS" AND ANY EXPRESS OR IMPLIED WARRANTIES, INCLUDING, BUT NOT
22  * LIMITED TO, THE IMPLIED WARRANTIES OF MERCHANTABILITY AND FITNESS FOR
23  * A PARTICULAR PURPOSE ARE DISCLAIMED. IN NO EVENT SHALL THE COPYRIGHT
24  * OWNER OR CONTRIBUTORS BE LIABLE FOR ANY DIRECT, INDIRECT, INCIDENTAL,
25  * SPECIAL, EXEMPLARY, OR CONSEQUENTIAL DAMAGES (INCLUDING, BUT NOT
26  * LIMITED TO, PROCUREMENT OF SUBSTITUTE GOODS OR SERVICES; LOSS OF USE,
27  * DATA, OR PROFITS; OR BUSINESS INTERRUPTION) HOWEVER CAUSED AND ON ANY
28  * THEORY OF LIABILITY, WHETHER IN CONTRACT, STRICT LIABILITY, OR TORT
29  * (INCLUDING NEGLIGENCE OR OTHERWISE) ARISING IN ANY WAY OUT OF THE USE
30  * OF THIS SOFTWARE, EVEN IF ADVISED OF THE POSSIBILITY OF SUCH DAMAGE.
31  */
32 
40 #ifndef MOD_NULL_H_
41 #define MOD_NULL_H_
42 
43 /* ========================================================================== */
44 /* Include Files */
45 /* ========================================================================== */
46 
47 #include <stdint.h>
49 #include <include/core/enet_mod.h>
51 
52 #ifdef __cplusplus
53 extern "C" {
54 #endif
55 
56 /* ========================================================================== */
57 /* Macros */
58 /* ========================================================================== */
59 
61 #define ENET_NULLMOD_FEAT1 (ENET_BIT(0U))
62 
64 #define ENET_NULLMOD_ERRATA1 (ENET_BIT(0U))
65 
67 #define ENET_NULLMOD_ERRATA2 (ENET_BIT(1U))
68 
69 /* ========================================================================== */
70 /* Structures and Enums */
71 /* ========================================================================== */
72 
76 typedef struct NullMod_Cfg_s
77 {
79  uint32_t dummy;
80 } NullMod_Cfg;
81 
85 typedef struct NullMod_Obj_s
86 {
89 } NullMod_Obj;
90 
94 typedef struct NullMod_Obj_s *NullMod_Handle;
95 
96 /* ========================================================================== */
97 /* Global Variables Declarations */
98 /* ========================================================================== */
99 
100 /* None */
101 
102 /* ========================================================================== */
103 /* Function Declarations */
104 /* ========================================================================== */
105 
113 void NullMod_initCfg(NullMod_Cfg *nullModCfg);
114 
129  Enet_Type enetType,
130  uint32_t instId,
131  const void *cfg);
132 
146  Enet_Type enetType,
147  uint32_t instId);
148 
161  uint32_t cmd,
162  Enet_IoctlPrms *prms);
163 
172 
173 
174 /* ========================================================================== */
175 /* Deprecated Function Declarations */
176 /* ========================================================================== */
177 
178 /* None */
179 
180 /* ========================================================================== */
181 /* Static Function Definitions */
182 /* ========================================================================== */
183 
184 /* None */
185 
186 #ifdef __cplusplus
187 }
188 #endif
189 
190 #endif /* MOD_NULL_H_ */
NullMod_initCfg
void NullMod_initCfg(NullMod_Cfg *nullModCfg)
Initialize Null module's configuration parameters.
NullMod_Handle
struct NullMod_Obj_s * NullMod_Handle
Null Module handle.
Definition: mod_null.h:94
NullMod_rejoin
int32_t NullMod_rejoin(EnetMod_Handle hMod, Enet_Type enetType, uint32_t instId)
Rejoin the Null Module.
enet_trace.h
This file contains the type definitions and helper macros for the Enet Trace interface.
NullMod_open
int32_t NullMod_open(EnetMod_Handle hMod, Enet_Type enetType, uint32_t instId, const void *cfg)
Open and initialize the Null Module.
NullMod_Obj::enetMod
EnetMod_Obj enetMod
Definition: mod_null.h:88
enet_types.h
This file contains the basic types using across the Enet driver.
Enet_IoctlPrms
Enet IOCTL param.
Definition: enet_ioctl.h:275
NullMod_Obj
Null Module object.
Definition: mod_null.h:86
EnetMod_Handle
struct EnetMod_Obj_s * EnetMod_Handle
Ethernet Module handle.
Definition: enet_mod.h:71
NullMod_ioctl
int32_t NullMod_ioctl(EnetMod_Handle hMod, uint32_t cmd, Enet_IoctlPrms *prms)
Issue an operation on the Null Module.
EnetMod_Obj
Ethernet Module object.
Definition: enet_mod.h:137
NullMod_Cfg
Null Module configuration parameters.
Definition: mod_null.h:77
Enet_Type
Enet_Type
Ethernet peripheral type.
Definition: enet_types.h:196
NullMod_close
void NullMod_close(EnetMod_Handle hMod)
Close the Null Module.
enet_mod.h
This file contains the type definitions and helper macros for the Enet Module interface.
NullMod_Cfg::dummy
uint32_t dummy
Definition: mod_null.h:79