![Logo](ti_logo.svg) |
AM243x MCU+ SDK
08.04.00
|
|
Go to the documentation of this file.
69 const uint8_t *packetData, int32_t packetLength, int32_t queuePriority);
83 const uint8_t *packetData, int32_t packetLength, int32_t queuePriority, int32_t port);
94 RED_FRAME *pRedFrame, int32_t portNumber, int32_t queuePriority);
struct ICSS_EMAC_Config_s * ICSS_EMAC_Handle
Alias for ICSS EMAC Handle containing base addresses and modules.
Definition: icss_emac.h:368
RED_STATUS RedTxPacketHsrModeT(ICSS_EMAC_Handle icssEmacHandle, const uint8_t *packetData, int32_t packetLength, int32_t queuePriority)
struct hsrPrp_Config_s hsrPrpHandle
Definition: hsrPrp_handle.h:92
Commonly used Macros, structures and Offsets.
RED_STATUS
RED Status.
Definition: hsrPrp_red_common.h:526
Include file for hsrPrp_red_hsr.c.
Definition: hsrPrp_red_common.h:146
RED_STATUS RedTxPacketHsrModeM(ICSS_EMAC_Handle icssEmacHandle, const uint8_t *packetData, int32_t packetLength, int32_t queuePriority, int32_t port)
RED_STATUS RedTxPacketEnqueue(hsrPrpHandle *, ICSS_EMAC_Handle icssEmacHandle, RED_FRAME *pRedFrame, int32_t portNumber, int32_t queuePriority)
Function to enqueue packet for transmission.