Affected API | Change |
---|---|
ENET_MDIO_IOCTL_GET_VERSION | Not Supported if MDIO is configured in Manual Mode |
ENET_MDIO_IOCTL_PRINT_REGS | Not Supported if MDIO is configured in Manual Mode |
ENET_MDIO_IOCTL_IS_ALIVE | Not Supported if MDIO is configured in Manual Mode |
ENET_MDIO_IOCTL_IS_LINKED | Not Supported if MDIO is configured in Manual Mode |
ENET_MDIO_IOCTL_IS_POLL_ENABLED | Not Supported if MDIO is configured in Manual Mode |
ENET_MDIO_IOCTL_C22_READ | Not Supported if MDIO is configured in Manual Mode |
ENET_MDIO_IOCTL_C22_WRITE | Not Supported if MDIO is configured in Manual Mode |
ENET_MDIO_IOCTL_C45_READ | Not Supported if MDIO is configured in Manual Mode |
ENET_MDIO_IOCTL_C45_WRITE | Not Supported if MDIO is configured in Manual Mode |
ENET_MDIO_IOCTL_C22_ASYNC_READ_TRIGGER | Not Supported if MDIO is configured in Manual Mode |
ENET_MDIO_IOCTL_C22_ASYNC_READ_COMPLETE | Not Supported if MDIO is configured in Manual Mode |
ENET_MDIO_IOCTL_C22_ASYNC_WRITE_TRIGGER | Not Supported if MDIO is configured in Manual Mode |
ENET_MDIO_IOCTL_C22_ASYNC_WRITE_COMPLETE | Not Supported if MDIO is configured in Manual Mode |
ENET_MDIO_IOCTL_C45_ASYNC_READ_TRIGGER | Not Supported if MDIO is configured in Manual Mode |
ENET_MDIO_IOCTL_C45_ASYNC_READ_COMPLETE | Not Supported if MDIO is configured in Manual Mode |
ENET_MDIO_IOCTL_C45_ASYNC_WRITE_TRIGGER | Not Supported if MDIO is configured in Manual Mode |
ENET_MDIO_IOCTL_C45_ASYNC_WRITE_COMPLETE | Not Supported if MDIO is configured in Manual Mode |
MDIO_IOCTL_HANDLE_INTR | Not Supported if MDIO is configured in Manual Mode |
ENET_MDIO_IOCTL_ENABLE_STATE_MACHINE | Not Supported if MDIO is configured in Manual Mode |