AM243x MCU+ SDK  08.04.00
EtherNet/IP Adapter Demos

Introduction

These examples are EtherNet/IP Adapter applications based on evaluation stacks provided in the SDK. Links to important sections in the detailed documentation are provided below:

Attention
If you need to reload and run the example again, EVM power-cycle is MUST.
Note
The work-around for issue "i2329 - MDIO: MDIO interface corruption (CPSW and PRU-ICSS)" (described in AM64x/AM243x Processor Silicon Revision 1.0, 2.0 (Rev. E)) is not available for this example in this release. It will be available in next release.

Supported Combinations

Parameter Value
CPU + OS r5fss0-0 freertos
ICSSG ICSSG1
Toolchain ti-arm-clang
Boards am243x-evm, am243x-lp (E1/E2 Revision)
Example folder examples/industrial_comms/ethernetip_adapter_demo
Note
This example will not work on PG2.0 HS-FS devices.