Struct for FWHAL initialization Parameters.
Data Fields | |
PRUICSS_Handle | pruicss_handle |
int32_t | interrupt_offset |
bsp_eeprom_read_t | eeprom_read |
bsp_eeprom_write_t | eeprom_write |
uint32_t | spinlock_base_address |
bsp_ethphy_init_t | ethphy_init |
uint8_t | enhancedlink_enable |
uint32_t | link0_polarity |
uint32_t | link1_polarity |
uint32_t | phy0_address |
uint32_t | phy1_address |
const unsigned char * | default_tiesc_eeprom |
uint8_t ** | eeprom_pointer_for_stack |
bsp_ethercat_stack_isr_function | pdi_isr |
bsp_ethercat_stack_isr_function | sync0_isr |
bsp_ethercat_stack_isr_function | sync1_isr |
uint16_t | phy_rx_err_reg |
uint8_t | pruicssClkFreq |
PRUICSS_Handle bsp_params::pruicss_handle |
PRUICSS Handle
int32_t bsp_params::interrupt_offset |
Interrupt Input Line number on ARM processor for PRU_ICSSG_PR1_HOST_INTR_PEND_0 interrupt. Out of 8 interrupts PRU_ICSSG_PR1_HOST_INTR_PEND_0 to PRU_ICSSG_PR1_HOST_INTR_PEND_7, following 4 are used for EtherCAT:
PRU_ICSSG_PR1_HOST_INTR_PEND_1 : DC SYNC0 OUT
PRU_ICSSG_PR1_HOST_INTR_PEND_2 : DC SYNC1 OUT
PRU_ICSSG_PR1_HOST_INTR_PEND_3 : PDI Interrupt
PRU_ICSSG_PR1_HOST_INTR_PEND_4 : ESC Command Acknowledgement
bsp_eeprom_read_t bsp_params::eeprom_read |
Function pointer to EEPROM Read function
bsp_eeprom_write_t bsp_params::eeprom_write |
Function pointer to EEPROM Read function
uint32_t bsp_params::spinlock_base_address |
Base address for HW spinlock. This is needed to prevent concurrent Host/Firmware shared memory access while reading latch timestamps.
bsp_ethphy_init_t bsp_params::ethphy_init |
Callback function for EtherCAT specific Ethernet PHY initialization
uint8_t bsp_params::enhancedlink_enable |
Enable enhanced link detection using MII RXLINK and PHY's enhanced link detection features. TIESC_MDIO_RX_LINK_ENABLE for enable, TIESC_MDIO_RX_LINK_DISABLE for disable
uint32_t bsp_params::link0_polarity |
Link Polarity for Port 0
uint32_t bsp_params::link1_polarity |
Link Polarity for Port 1
uint32_t bsp_params::phy0_address |
Ethernet PHY Address for Port 0
uint32_t bsp_params::phy1_address |
Ethernet PHY Address for Port 1
const unsigned char* bsp_params::default_tiesc_eeprom |
Pointer to EEPROM array corresponding to ESI XML
uint8_t** bsp_params::eeprom_pointer_for_stack |
Double pointer to eeprom variable which will be used by stack. bsp_init will populate this pointer appropriately
bsp_ethercat_stack_isr_function bsp_params::pdi_isr |
PDI IRQ handler in the EtherCAT slave stack. Needed only if ENABLE_PDI_TASK is not enabled
bsp_ethercat_stack_isr_function bsp_params::sync0_isr |
SYNC0 IRQ handler in the EtherCAT slave stack. Needed only if ENABLE_SYNC_TASK is not enabled
bsp_ethercat_stack_isr_function bsp_params::sync1_isr |
SYNC1 IRQ handler in the EtherCAT slave stack. Needed only if ENABLE_SYNC_TASK is not enabled
uint16_t bsp_params::phy_rx_err_reg |
Address of PHY register maintaining RX Error (RX_ERR) count during frame(when RX_DV is asserted). This value will be configured in TI ESC's PHY RX Error Counter Register (0x0E28-0x0E29)
uint8_t bsp_params::pruicssClkFreq |
PRU-ICSS Core Clock and IEP Clock Frequency. Set TIESC_PRUICSS_CLOCK_FREQUENCY_200_MHZ/TIESC_PRUICSS_CLOCK_FREQUENCY_333_MHZ. Default is TIESC_PRUICSS_CLOCK_FREQUENCY_200_MHZ. NOTE : Only applicable for PRU-ICSSG (AM64x/AM243x). Not applicable for PRU-ICSSM(AM263x).