Features Supported
- APIs to create and destroy Queues
- APIs to Put element in Queue
- APIs to Get element from Queue
- APIs to Check if Queue is Empty
Features NOT Supported
NA
Important Usage Guidelines
- For creating the Queue application needs to provide the QueueP_Object and it should not be modified by the applicaion.
- A field of type QueueP_Elem should be placed at the head of client structs passed as Queue Elements to function QueueP_put.
- It is recommended not to place the QueueP Object and QueueP Element objects in stack as they will be accessed by the driver till they are released.
Example Usage
Include the below file to access the APIs,
Example usage define Queue Object and Elements
typedef struct Test_Queue_Elem_s
{
} Test_Queue_Elem;
Test_Queue_Elem elem1, elem2;
Example to Create and use the Queue
API
APIs for Queue