The ICSS TimeSync driver provide APIs for PTP/1588 v2 slave implementation on PRU-ICSS.
Precision Time Protocol (PTP) comes in a variety of standards and flavors. Every industry has it's own set of sub rules and configurations which are defined by Annexes and Profiles. For example, the telecom industry uses the telecom profile, while power and substation automation requires the power profile. CIP sync requires the Drive profile.
Keeping above points in mind, ICSS TimeSync driver provides support for following flavor :
Delay Request/Response based Ordinary Clock and Transparent Clock support is provided to support CIP Sync, which requires support for Annex D of PTP/1588 (PTP over UDP).
ICSS TimeSync Design explains the driver design in detail.
Include the below file to access the APIs
TimeSync_drvInit should be called initialize the driver. It does everything and returns a value indicating whether initialization succeeded or failed. The driver call does not allocate the memory it needs. Therefore the allocation must be done by the application.
The variables shown in the code above do not show the full list of configurable variables and structures for which memory should be allocated. Please check all members inside TimeSync_ParamsHandle structure.
A separate call is required to TimeSync_drvEnable is needed for enabling PTP processing in firmware. The corresponding TimeSync_drvDisable call disables the module in firmware.
TimeSync_addIP should be called to update IP and modify checksum in PTP packet buffers, whenever IP is assigned or changed.
Porting your own PTP/1588 stack is simple because most of the tasks, especially the time critical tasks are performed by the driver. The stack is only responsible for
Once TimeSync_drvInit and TimeSync_drvEnable APIs are called from the application, all PTP announce and management messages are sent on the highest priority queue to the host. All incoming PTP frames are handled through the regular Rx interrupt registered by ICSS-EMAC (See Interrupts section in ICSS-EMAC Design for more details). TimeSync_processPTPFrame must be called for processing PTP frames. As mentioned in Rx Data Path, rxRTCallBack needs to be registered to process these frames in queues. Therefore, either TimeSync_processPTPFrame must be registered as rxRTCallBack, or if different types of frames (other than PTP) are coming on the high priority queues, then application must differentiate PTP frames in rxRTCallBack and then call the TimeSync_processPTPFrame API for PTP frames.
In TimeSync_processPTPFrame, the frame type is checked and if it is an Announce or Management message the data is copied to the buffer ptpGeneralFrame. Once the frame has been copied a flag generalFrameFlag is set. Another API called TimeSync_getGeneralMessage checks the flag and copies the data from the buffer ptpGeneralFrame to another buffer buff which belongs to the PTP stack. The API TimeSync_getGeneralMessage strips the header from the frame based on whether the mode is E2E or P2P and only copies the relevant data to the stack buffer. This way only the relevant data is sent to stack and stack need not worry whether the mode is E2E or P2P.
The stack can either modify TimeSync_processPTPFrame to call the TimeSync_getGeneralMessage API, or call TimeSync_getGeneralMessage in a loop in a task.
PRU-ICSS firmware compares the Source MAC ID of Sync and Follow Up frames with the value stored at the offset PTP_MASTER_SRC_MAC_ID in PRU-ICSS Shared RAM, and if it does not match then the sync processing does not happen. For starting sync processing, BMCA has to complete and once the source MAC ID of a master is available, it should be shared with firmware by calling TimeSync_updateParentAddress.
As explained in Timestamping section of ICSS TimeSync Design page, ICSS TimeSync has a very simple design where the IEP counter acts as the nanoseconds counter. TimeSync_getCurrentTime returns the current time on device.
In case of a timeout, link break, etc. the driver requires a reset. This is done using the TimeSync_reset. This API also calls the TimeSync_stackResetCallback_t which can be registered by stack.
Most of the information related to PTP is encapsulated in Announce and Management messages. However certain information is part of the driver, and the stack may need access to these for its operation. Relevant information can be read from the runtime structure timeSync_RuntimeVar_t based on the requirement.
Internal structures used by ICSS TimeSync Driver can be checked for debugging. Most relevant structures are timeSync_RuntimeVar_t are timeSync_SyntInfo_t.