AM243x MCU+ SDK  08.03.00
Profinet Device Demos

Introduction

Examples for Profinet Device RT (Conformance Class - B) based on evaluation stacks provided in the SDK. Links to important sections in the detailed documentation are provided below:

Attention
If you need to reload and run the example again, EVM power-cycle is MUST.

Supported Combinations

Parameter Value
CPU + OS r5fss0-0 freertos
ICSSG ICSSG1
Toolchain ti-arm-clang
Boards am243x-evm, am243x-lp
Example folder examples/industrial_comms/profinet_device_demo