Ethernet Interface
Modules | |
Ethernet Interface Error Codes | |
Functions | |
uint32_t | PN_API_ETH_applyConfiguration (const PN_API_ETH_SConfiguration_t *pConfiguration_p) |
Apply configuration of ethernet interface. More... | |
uint32_t | PN_API_ETH_applyPermanentDcpData (const PN_API_ETH_SPermanentDcpData_t *pData_p) |
Apply permanent DCP data of ethernet interface. More... | |
uint32_t | PN_API_ETH_applyPermanentPortData (const PN_API_ETH_SPermanentPortData_t *pData_p) |
Apply permanent port data of ethernet interface. More... | |
uint32_t | PN_API_ETH_getPortLinkState (PN_API_ETH_EPort_t port_p, PN_API_ETH_EPortLinkState_t *pState_p) |
Get link state of ethernet interface port. More... | |
uint32_t | PN_API_ETH_getPortMauType (PN_API_ETH_EPort_t port_p, PN_API_ETH_EPortMauType_t *pType_p) |
Get media access unit (MAU) type of ethernet interface port. More... | |
uint32_t | PN_API_ETH_getStationName (const uint8_t **ppName_p, uint16_t *pLength_p) |
Get station name of ethernet interface. More... | |