Overview
The Software Development Kit (SDK) for EtherCAT allows you to quickly integrate EtherCAT slave functionality into your device. The SDK is supported for Sitara processors by Texas Instruments Incorporated and currently available for AM64x and AM243x series of Cortex®-R5 based devices.
This document collection contains a Quickstart Guide, the User Manual, and the API Reference Manual for the EtherCAT Slave SDK. The API consists of the following modules: an API to access the basic EtherCAT Slave functionality, the API for the CiA 402 (Drives and Motion Control), the cyclic buffer handling API, and a board support package API.
Licensing
Copyright ©2021, KUNBUS GmbH
All rights reserved.
Redistribution and use in source and binary forms, with or without modification, are permitted provided that the following conditions are met:
-
Redistributions of source code must retain the above copyright notice, this list of conditions and the following disclaimer.
-
Redistributions in binary form must reproduce the above copyright notice, this list of conditions and the following disclaimer in the documentation and/or other materials provided with the distribution.
-
Neither the name of the copyright holder nor the names of its contributors may be used to endorse or promote products derived from this software without specific prior written permission.
THIS SOFTWARE IS PROVIDED BY THE COPYRIGHT HOLDERS AND CONTRIBUTORS "AS IS" AND ANY EXPRESS OR IMPLIED WARRANTIES, INCLUDING, BUT NOT LIMITED TO, THE IMPLIED WARRANTIES OF MERCHANTABILITY AND FITNESS FOR A PARTICULAR PURPOSE ARE DISCLAIMED. IN NO EVENT SHALL THE COPYRIGHT HOLDER OR CONTRIBUTORS BE LIABLE FOR ANY DIRECT, INDIRECT, INCIDENTAL, SPECIAL, EXEMPLARY, OR CONSEQUENTIAL DAMAGES (INCLUDING, BUT NOT LIMITED TO, PROCUREMENT OF SUBSTITUTE GOODS OR SERVICES; LOSS OF USE, DATA, OR PROFITS; OR BUSINESS INTERRUPTION) HOWEVER CAUSED AND ON ANY THEORY OF LIABILITY, WHETHER IN CONTRACT, STRICT LIABILITY, OR TORT (INCLUDING NEGLIGENCE OR OTHERWISE) ARISING IN ANY WAY OUT OF THE USE OF THIS SOFTWARE, EVEN IF ADVISED OF THE POSSIBILITY OF SUCH DAMAGE.
Release Version 1.06.01
New Features:
-
[DTKEC-693] Build SSC Libary with EC patch standalone
Provide a patch for users to build the Beckhoff SSC Library with support for non-evaluation hardware.
-
[DTKEC-301] Test SDKon AM243x EVM Hardware
Stack on AM243x EVM passed ETG conformance tool automated tests.
-
[DTKEC-732] Integrate documentation of the OBD and Process Data configuration in Doxygen
Extended documentation from ETG documents. See chapter EtherCAT SDKFAQ.
Bugfix:
-
[DTKEC-742] Improve firmware load stability on AM243EVM and AM64EVM
- a former need call has been removed, which makes download of EtherCAT SDKmore likely successful
-
[DTKEC-730] Build Warning still prevalent on the AM243x LP
Removed duplicate definitions from board config code.
-
[DTKEC-731] Solve issue of loading firmware to the core
Removed stale MPU configuration entry from sysconfig for AM64x-EVM.
Release Version 1.06.00
New Features:
Bugfix:
-
[DTKEC-673] FreeRTOS debug support
- Fix linker files to make examples debugable again
- Reduce memory usage of IP protection security algorithms
-
[DTKEC-675] FreeRTOS thread stacks
- Move thread stack variables to dedicated linker / memory section to avoid overwrite from stack manager
Release Version 1.05.02
Bugfix:
-
[DTKEC-645] Version incorrectly displayed
- Incorrect version was displayed in the previous release.
Release Version 1.05.01
Bugfix:
-
[DTKEC-631] Datasheet memory information missing
- Minor documentation corrections
Release Version 1.05.00
New Features:
-
[DTKEC-573] MCU+SDK 8.01.00.35
- Update to MCU+SDK 8.01.00.35
-
[DTKEC-342] Protection of intelectual property
- Add new chip based license verification
Release Version 1.04.06
New Features:
-
[DTKEC-528] MCU+SDK 8.01.00.26
- Update to MCU+SDK 8.01.00.26
- Use Code Composer 11
Release Version 1.04.05
New Features:
-
[DTKEC-474] Documentation
- Update datasheet and add key performance parameter information
- Remove references to SDKAPI from CiA-402 example
- Fixed hyperlinks from Simple example documentation
-
[DTKEC-473] SysConfig AM243-EVM
Remove obsolete DDR4 RAM entry from MPU configuration on AM64-EVM and AM243-EVM
-
[DTKEC-472] Analyze library size differences
Use optimization for linkage Oz for all MCUs on FreeRTOS
Release Version 1.04.04
New Features:
-
[DTKEC-477] Automatic versioning
Add automatic global versioning to demo apps and remove some compile time warning.
-
[DTKEC-448] Documentation automation
Add size measurement to documentation
-
[DTKEC-403] Performance improvement
Add measurement callback functions and additional APIs which allow to directly access CoE objects to improve performance while accessing objects in control cycle (e.g. CiA 402).
-
[DTKEC-455] Remove next steps to build an example
Build an example description removed from documentation and replaced by Steps to Run the Example.
Release Version 1.04.03
New Features:
-
[DTKEC-372] Move "Supported Functionality" to the top level
The "Supported Functionality" section in the documentation has been moved from "General Information" to the top-level.
-
[DTKEC-402] Project name change
The project name has been changed from ethercat_linux to product_ethercat_slave.
-
[DTKEC-381] Reduce memory footprint
Stack is now compiled with THUMB mode. Additionally, the ESI parser has been moved to the application.
-
[DTKEC-394] Suppress linker warnings
The linker warnings have been corrected.
-
[DTKEC-395] OSAL_error 0x40000001 EC
Missing defines have been added to TI shipped example.projectspec(s) accordingly
-
[DTKEC-396] MCU+ SDK 8.01.00.10 Support
EtherCAT SDKhas been updated to support MCU+SDK 8.01.00.10.
-
[DTKEC-398] AM243x Heap size
The heap size for the AM243x applications has been reduced.
Release Version 1.04.02
New Features:
-
[DTKEC-343] MCU+SDK 8.01.00.02 Support
MCU+SDK 8.01.0.02 is now supported.
-
[DTKEC-243] Run and Error LED migrated TEST_LED_1 and TEST_LED_2
The run and error LEDs have been migrated to TEST_LED_1 and TEST_LED_2, respectively.
-
[DTKEC-167] Memory allocation reduction
The dynamically allocated memory footprint of the stack has been reduced. Additionally, the stack
memory access has been migrated from DDR to MSRAM.
Bug Fixes:
-
[DTKEC-348] Both ports not working with AM243x LP
Corrected issue with no communication on the second port.
-
[DTKEC-334] Update linker files to load apps only from MSRAM
The linker scripts were not fully adjusted to support MSRAM. This has been corrected.
-
[DTKEC-318] Repeating "Data Transfer failed with transfer status -2" Message
The "Data Transfer failed with transfer status -2" message that repeatedly displayed in the console output has been resolved.
Release Version 1.04.01
New Features:
-
[DTKEC-303] Create Project for AM243X EVM
Created new Code Composer Studio project for AM243X EVM and created documentation for the new platform.
Bug Fixes:
-
[DTKEC-317] Fix startup stability issue
Allocation of the stack size has been changed to the expected value. The larger size led to instabilities while booting up.
Release Version 1.04.00
New Features:
-
[DTKEC-256] MCU+SDK 08.00.00.08 Support
EtherCAT SDKhas been updated to support MCU+SDK 08.00.00.08.
-
[DTKEC-283] Create Project for AM24X
Created new Code Composer Studio project for AM243 and created documentation for the new platform.
Bug Fixes:
-
[DTKEC-250] Fix ESI file content for Simple, CTT and CIA402
Corrected inconsistencies between all ESI files.
-
[DTKEC-247] AM64x ESI file fix
Corrected access to PDO Mapping.
Release Version 1.03.01
New Features:
-
[DTKEC-237] AM64 Demo refactoring
Split of OS and MCU support files in DemoApps
Add conformance test tool Demo sources
Add CiA402 Demo sources
Release Version 1.03.00
New Features:
-
[DTKEC-162] CiA402 3 axes application example
Configuration of the CiA402 Object Dictionary and Process Data mapping described on ETG6010 Chapter 11 & 16.
ESI File (EtherCAT Device Description file) for the CiA402 example.
CiA402 state machine test. CiA402 is based on a state machine described in ETG6010 Chapter 5.
Bug Fixes:
-
[DTKEC-228] AM64 Startup problems corrected
Updated to support MCUplus 7.3.1.07.
Release Version 1.02.03
New Features:
-
[P2102-1] EtherCAT AM64 Porting to FreeRTOS
Support for FreeRTOS R5 on AM64 controller has been added. Tickets included: P2101-2->9; P2101-11->16; P2101-19->29
Release Version 1.02.00
New Features:
Release Version 1.01.01
New Features:
-
Abstraction Layer baseline adopted in order to migrate to SDK7 in next Release
Release Version 1.01.00
New Features: