|
typedef void(* | EC_API_SLV_CBBoardPhyReset_t) (void *pContext_p, uint8_t phyIdx_p, bool resetActive_p) |
| Handle PHY reset line. More...
|
|
typedef void(* | EC_API_SLV_CBBoardStatusLed_t) (void *pContext_p, void *pLedContext_p, bool errLed_p, bool statusLed_p) |
| Set Status LED call back. More...
|
|
typedef void(* | EC_API_SLV_CBPhySpecific_SoftReset_t) (void *pAppContext_p, void *pStackContext_p, uint32_t phyAddr_p) |
| Issue PHY Reset by software (used if no Hard Reset is available) More...
|
|
typedef void(* | EC_API_SLV_CBPhySpecific_softRestart_t) (void *pAppContext_p, void *pStackContext_p, uint32_t phyAddr_p) |
| Issue PHY restart by software. More...
|
|
typedef void(* | EC_API_SLV_CBPhySpecific_EnableAutoMDIX_t) (void *pAppContext_p, void *pStackContext_p, uint32_t phyAddr_p) |
| Enable Auto MDIX. More...
|
|
typedef void(* | EC_API_SLV_CBPhySpecific_SetMIIMode_t) (void *pAppContext_p, void *pStackContext_p, uint32_t phyAddr_p) |
| Set MII Mode. More...
|
|
typedef void(* | EC_API_SLV_CBPhySpecific_SetPowerModeT) (void *pAppContext_p, void *pStackContext_p, uint32_t phyAddr_p, bool powerDown_p) |
| Configure PhyMLED to detect RxLink by MLED (e.g. TLK) More...
|
|
typedef bool(* | EC_API_SLV_CBPhySpecific_GetPowerMode_t) (void *pAppContext_p, void *pStackContext_p, uint32_t phyAddr_p) |
| Provides Phy power mode state. More...
|
|
typedef void(* | EC_API_SLV_CBPhySpecific_MLEDConfig_t) (void *pAppContext_p, void *pStackContext_p, uint32_t phyAddr_p) |
| Configure PhyMLED to detect RxLink by MLED (e.g. TLK) More...
|
|
typedef void(* | EC_API_SLV_CBPhySpecific_ExtFDEnable_t) (void *pAppContext_p, void *pStackContext_p, uint32_t phyAddr_p) |
| Set Ext Full Duplex enable. More...
|
|
typedef void(* | EC_API_SLV_CBPhySpecific_ODDNibbleDetEnable_t) (void *pAppContext_p, void *pStackContext_p, uint32_t phyAddr_p) |
| Set ODD Nibble detection enable. More...
|
|
typedef void(* | EC_API_SLV_CBPhySpecific_RxErrIdleEnable_t) (void *pAppContext_p, void *pStackContext_p, uint32_t phyAddr_p) |
| Set Rx Error Idle enable. More...
|
|
typedef void(* | EC_API_SLV_CBPhySpecific_LedConfig_t) (void *pAppContext_p, void *pStackContext_p, uint32_t phyAddr_p) |
| Configure PHY LEDs. More...
|
|
typedef void(* | EC_API_SLV_CBPhySpecific_LedBlinkConfig_t) (void *pAppContext_p, void *pStackContext_p, uint32_t phyAddr_p) |
| Configure PHY Blink LED mode. More...
|
|
typedef void(* | EC_API_SLV_CBPhySpecific_FastLinkDownDetEnable_t) (void *pAppContext_p, void *pStackContext_p, uint32_t phyAddr_p) |
| Set fast link down Detection enable. More...
|
|
typedef void(* | EC_API_SLV_CBPhySpecific_FastRXDVDetEnable_t) (void *pAppContext_p, void *pStackContext_p, uint32_t phyAddr_p) |
| Set Fast RX DV detection enable. More...
|
|
typedef void(* | EC_API_SLV_CBPhySpecific_SwStrapConfigDone_t) (void *pAppContext_p, void *pStackContext_p, uint32_t phyAddr_p) |
| Set SW Strap config done. More...
|
|
typedef void(* | EC_API_SLV_CBPhySpecific_setLinkConfig_t) (void *pAppContext_p, void *pStackContext_p, uint32_t phyAddr_p, bool autoNeg_p, uint16_t linkSpeed_p, bool fullDuplex_p, uint32_t *pResult_p) |
| Configures PHY for link connection. More...
|
|
typedef bool(* | EC_API_SLV_CBPhySpecific_getAutoNegotiation_t) (void *pAppContext_p, void *pStackContext_p, uint32_t phyAddr_p) |
| Provides auto-negotiation enabled flag. More...
|
|
typedef void(* | EC_API_SLV_CBPhySpecific_setMdixMode_t) (void *pAppContext_p, void *pStackContext_p, uint32_t phyAddr_p, uint32_t mdixMode_p) |
| Configures PHY MDI crossover mode. More...
|
|
typedef uint32_t(* | EC_API_SLV_CBPhySpecific_getMdixMode_t) (void *pAppContext_p, void *pStackContext_p, uint32_t phyAddr_p) |
| Provides actually used PHY MDI crossover mode. More...
|
|
typedef void(* | EC_API_SLV_CBPhySpecific_disable1GbAdver_t) (void *pAppContext_p, void *pStackContext_p, uint32_t phyAddr_p) |
| Disables 1Gbit Advertisment during autonegotiation. More...
|
|
typedef void(* | EC_API_SLV_CBPhySpecific_rgmiiLowLatencyEnable_t) (void *pAppContext_p, void *pStackContext_p, uint32_t phyAddr_p) |
| Enables low latency in RGMII mode. More...
|
|
typedef void(* | EC_API_SLV_CBPhySpecific_rgmiiTxHalfFullThreshold_t) (void *pAppContext_p, void *pStackContext_p, uint32_t phyAddr_p, uint32_t threshold_p) |
| RGMII_TX_HALF_FULL_THR[1:0] can be changed from the default of 0x2 to 0x1. This will reduce the latency by one clock period. More...
|
|
typedef void(* | EC_API_SLV_CBPhySpecific_rgmiiRxHalfFullThreshold_t) (void *pAppContext_p, void *pStackContext_p, uint32_t phyAddr_p, uint32_t threshold_p) |
| RGMII_RX_HALF_FULL_THR[1:0] can be changed from the default of 0x2 to 0x1. This will reduce the latency by one clock period. More...
|
|
typedef struct EC_API_SLV_SPhyDescriptor | EC_API_SLV_SPhyDescriptor_t |
|
typedef int16_t(* | EC_API_SLV_CBExtPhyLibDetect_t) (void *pPhyLibCtxt_p, uint8_t phyIdx_p, uint32_t phyId_p, uint8_t phyAddr_p, EC_API_SLV_SPhyDescriptor_t *pPhyLibDesc_p) |
| Phy Detection callback of external PhyLib. More...
|
|