![Logo](ti_logo.svg) |
AM243x MCU+ SDK
08.02.00
|
|
Go to the documentation of this file.
84 #define CPSW_CPTS_PUBLIC_IOCTL(x) (ENET_IOCTL_TYPE_PUBLIC | \
85 ENET_IOCTL_TIMESYNC_BASE | \
86 ENET_IOCTL_PER_CPSW | \
90 #define CPSW_CPTS_NUDGE_MIN_VAL (-128)
93 #define CPSW_CPTS_NUDGE_MAX_VAL (127)
102 typedef enum CpswCpts_Ioctl_s
228 typedef enum CpswCpts_RftClkFreq_e
258 typedef enum CpswCpts_EventType_e
291 typedef enum CpswCpts_OutputBitSel_e
345 typedef enum CpswCpts_HwPush_e
382 #define CPSW_CPTS_HWPUSH_COUNT_MAX ((uint32_t)CPSW_CPTS_HWPUSH_LAST)
385 #define CPSW_CPTS_HWPUSH_NORM(x) ((uint32_t)((x) - CPSW_CPTS_HWPUSH_FIRST))
390 typedef struct CpswCpts_Event_s
439 typedef struct CpswCpts_StackConfig_s
451 typedef struct CpswCpts_RegisterHwPushCbInArgs_s
466 typedef struct CpswCpts_SetCompValInArgs_s
484 typedef struct CpswCpts_SetFxnGenInArgs_s
516 typedef struct CpswCpts_SetFxnGenNudgeInArgs_s
531 typedef struct CpswCpts_Cfg_s
Input args for CPSW_CPTS_IOCTL_REGISTER_STACK command.
Definition: cpsw_cpts.h:440
uint32_t index
Definition: cpsw_cpts.h:519
@ CPSW_CPTS_IOCTL_SET_GENF_NUDGE
CPTS set GenFn stamp nudge.
Definition: cpsw_cpts.h:186
@ CPSW_CPTS_HWPUSH_5
Definition: cpsw_cpts.h:363
bool tsCompPolarity
Definition: cpsw_cpts.h:540
@ CPSW_CPTS_IOCTL_SET_GENF
CPTS set function generator.
Definition: cpsw_cpts.h:177
void * eventNotifyCbArg
Definition: cpsw_cpts.h:445
@ CPSW_CPTS_IOCTL_UNREGISTER_STACK
CPTS unregister stack.
Definition: cpsw_cpts.h:120
@ CPSW_CPTS_RFTCLK_FREQ_125MHZ
Definition: cpsw_cpts.h:252
bool tsRxEventsDis
Definition: cpsw_cpts.h:543
@ CPSW_CPTS_EVENTTYPE_ETH_RECEIVE
Definition: cpsw_cpts.h:273
@ CPSW_CPTS_EVENTTYPE_TS_ROLLOVER
Definition: cpsw_cpts.h:264
@ CPSW_CPTS_HWPUSH_INVALID
Definition: cpsw_cpts.h:378
Input args for CPSW_CPTS_IOCTL_SET_COMP command.
Definition: cpsw_cpts.h:467
void(* CpswCpts_EventNotifyCb)(void *eventNotifyCbArg, CpswCpts_Event *eventInfo)
CPTS event notify callback.
Definition: cpsw_cpts.h:421
@ CPSW_CPTS_TS_OUTPUT_BIT_29
Definition: cpsw_cpts.h:333
@ CPSW_CPTS_HWPUSH_FIRST
Definition: cpsw_cpts.h:348
uint64_t ppmVal
Definition: cpsw_cpts.h:501
@ CPSW_CPTS_EVENTTYPE_INVALID
Definition: cpsw_cpts.h:285
@ CPSW_CPTS_TS_OUTPUT_BIT_23
Definition: cpsw_cpts.h:315
@ CPSW_CPTS_RFTCLK_FREQ_1000MHZ
Definition: cpsw_cpts.h:231
CpswCpts_HwPush hwPushNum
Definition: cpsw_cpts.h:454
bool polarityInv
Definition: cpsw_cpts.h:498
int32_t tsNudge
Definition: cpsw_cpts.h:523
@ CPSW_CPTS_IOCTL_REGISTER_HWPUSH_CALLBACK
CPTS register hardware push event callback.
Definition: cpsw_cpts.h:129
EnetTimeSync_MsgType msgType
Definition: cpsw_cpts.h:399
@ CPSW_CPTS_TS_OUTPUT_BIT_28
Definition: cpsw_cpts.h:330
@ CPSW_CPTS_TS_OUTPUT_BIT_17
Definition: cpsw_cpts.h:297
@ CPSW_CPTS_HWPUSH_1
Definition: cpsw_cpts.h:351
@ CPSW_CPTS_RFTCLK_FREQ_200MHZ
Definition: cpsw_cpts.h:243
@ CPSW_CPTS_EVENTTYPE_TS_PUSH
Definition: cpsw_cpts.h:261
@ CPSW_CPTS_EVENTTYPE_TS_HOST_TX
Definition: cpsw_cpts.h:282
@ CPSW_CPTS_IOCTL_SET_ESTF_NUDGE
CPTS set ESTFn stamp nudge.
Definition: cpsw_cpts.h:204
CpswCpts_HwPushNotifyCb hwPushNotifyCb
Definition: cpsw_cpts.h:457
@ CPSW_CPTS_HWPUSH_LAST
Definition: cpsw_cpts.h:375
@ CPSW_CPTS_TS_OUTPUT_BIT_25
Definition: cpsw_cpts.h:321
CpswCpts_OutputBitSel
CPTS time stamp output bit.
Definition: cpsw_cpts.h:292
@ CPSW_CPTS_HWPUSH_3
Definition: cpsw_cpts.h:357
@ CPSW_CPTS_TS_OUTPUT_BIT_26
Definition: cpsw_cpts.h:324
@ CPSW_CPTS_IOCTL_SET_ESTF
CPTS set EST function generator.
Definition: cpsw_cpts.h:195
uint32_t length
Definition: cpsw_cpts.h:490
@ CPSW_CPTS_IOCTL_REGISTER_STACK
CPTS register stack.
Definition: cpsw_cpts.h:111
@ CPSW_CPTS_HWPUSH_2
Definition: cpsw_cpts.h:354
bool hostRxTsEn
Definition: cpsw_cpts.h:535
Input args for CPSW_CPTS_IOCTL_SET_GENF and CPSW_CPTS_IOCTL_SET_ESTF commands.
Definition: cpsw_cpts.h:485
CPTS configuration.
Definition: cpsw_cpts.h:532
void * hwPushNotifyCbArg
Definition: cpsw_cpts.h:460
uint64_t tsVal
Definition: cpsw_cpts.h:393
@ CPSW_CPTS_IOCTL_UNREGISTER_HWPUSH_CALLBACK
CPTS unregister hardware push event callback.
Definition: cpsw_cpts.h:138
@ CPSW_CPTS_TS_OUTPUT_BIT_30
Definition: cpsw_cpts.h:336
CpswCpts_EventNotifyCb eventNotifyCb
Definition: cpsw_cpts.h:442
@ CPSW_CPTS_EVENTTYPE_TS_HALFROLLOVER
Definition: cpsw_cpts.h:267
#define CPSW_CPTS_PUBLIC_IOCTL(x)
Helper macro to create IOCTL commands for CPSW CPTS module.
Definition: cpsw_cpts.h:84
uint64_t tsCompVal
Definition: cpsw_cpts.h:469
CpswCpts_HwPush hwPushNum
Definition: cpsw_cpts.h:411
CpswCpts_HwPush
CPTS Hardware push instances.
Definition: cpsw_cpts.h:346
uint32_t index
Definition: cpsw_cpts.h:487
@ CPSW_CPTS_IOCTL_SET_COMP
CPTS set compare value.
Definition: cpsw_cpts.h:159
@ CPSW_CPTS_TS_OUTPUT_BIT_24
Definition: cpsw_cpts.h:318
uint32_t portNum
Definition: cpsw_cpts.h:405
void CpswCpts_initCfg(CpswCpts_Cfg *cptsCfg)
Initialize CPSW CPTS configuration parameters.
CpswCpts_Ioctl
CPSW CPTS IOCTL commands.
Definition: cpsw_cpts.h:103
@ CPSW_CPTS_HWPUSH_7
Definition: cpsw_cpts.h:369
@ CPSW_CPTS_EVENTTYPE_HW_TS_PUSH
Definition: cpsw_cpts.h:270
@ CPSW_CPTS_TS_OUTPUT_BIT_DISABLED
Definition: cpsw_cpts.h:294
@ CPSW_CPTS_HWPUSH_8
Definition: cpsw_cpts.h:372
@ CPSW_CPTS_HWPUSH_4
Definition: cpsw_cpts.h:360
Input args for CPSW_CPTS_IOCTL_REGISTER_HWPUSH_CALLBACK command.
Definition: cpsw_cpts.h:452
@ CPSW_CPTS_TS_OUTPUT_BIT_22
Definition: cpsw_cpts.h:312
@ CPSW_CPTS_TS_OUTPUT_BIT_31
Definition: cpsw_cpts.h:339
@ CPSW_CPTS_RFTCLK_FREQ_500MHZ
Definition: cpsw_cpts.h:234
@ CPSW_CPTS_TS_OUTPUT_BIT_20
Definition: cpsw_cpts.h:306
@ CPSW_CPTS_IOCTL_LOOKUP_EVENT
CPTS lookup event.
Definition: cpsw_cpts.h:222
EnetTimeSync_AdjMode
TimeSync adjustment mode.
Definition: enet_mod_timesync.h:205
@ CPSW_CPTS_RFTCLK_FREQ_250MHZ
Definition: cpsw_cpts.h:240
@ CPSW_CPTS_TS_OUTPUT_BIT_21
Definition: cpsw_cpts.h:309
EnetTimeSync_AdjDir ppmDir
Definition: cpsw_cpts.h:504
uint64_t compare
Definition: cpsw_cpts.h:493
@ CPSW_CPTS_HWPUSH_6
Definition: cpsw_cpts.h:366
This file contains the type definitions and helper macros for the Enet Time Synchronization module in...
@ CPSW_CPTS_EVENTTYPE_ETH_TRANSMIT
Definition: cpsw_cpts.h:276
CpswCpts_EventType
CPTS event type.
Definition: cpsw_cpts.h:259
CpswCpts_EventType eventType
Definition: cpsw_cpts.h:396
@ CPSW_CPTS_EVENTTYPE_TS_COMP
Definition: cpsw_cpts.h:279
uint32_t domain
Definition: cpsw_cpts.h:408
Input args for CPSW_CPTS_IOCTL_SET_GENF_NUDGE and CPSW_CPTS_IOCTL_SET_ESTF_NUDGE commands.
Definition: cpsw_cpts.h:517
EnetTimeSync_AdjDir
TimeSync adjustment direction.
Definition: enet_mod_timesync.h:220
@ CPSW_CPTS_RFTCLK_FREQ_333_33MHZ
Definition: cpsw_cpts.h:237
void(* CpswCpts_HwPushNotifyCb)(void *hwPushNotifyCbArg, CpswCpts_HwPush hwPushNum)
CPTS hardware push notify callback/.
Definition: cpsw_cpts.h:431
@ CPSW_CPTS_TS_OUTPUT_BIT_18
Definition: cpsw_cpts.h:300
@ CPSW_CPTS_IOCTL_SET_COMP_NUDGE
CPTS set compare nudge.
Definition: cpsw_cpts.h:168
@ CPSW_CPTS_TS_OUTPUT_BIT_19
Definition: cpsw_cpts.h:303
@ CPSW_CPTS_IOCTL_SELECT_TS_OUTPUT_BIT
CPTS TS output bit select.
Definition: cpsw_cpts.h:213
@ CPSW_CPTS_RFTCLK_FREQ_142_85MHZ
Definition: cpsw_cpts.h:249
EnetTimeSync_MsgType
TimeSync Ethernet message type.
Definition: enet_mod_timesync.h:166
bool tsCompToggle
Definition: cpsw_cpts.h:477
CpswCpts_RftClkFreq
CPTS clock frequency add value.
Definition: cpsw_cpts.h:229
@ CPSW_CPTS_RFTCLK_FREQ_166_66MHZ
Definition: cpsw_cpts.h:246
CpswCpts_RftClkFreq cptsRftClkFreq
Definition: cpsw_cpts.h:553
uint32_t tsCompLen
Definition: cpsw_cpts.h:472
@ CPSW_CPTS_TS_OUTPUT_BIT_27
Definition: cpsw_cpts.h:327
CPTS event.
Definition: cpsw_cpts.h:391
bool tsGenfClrEn
Definition: cpsw_cpts.h:550
EnetTimeSync_AdjMode ppmMode
Definition: cpsw_cpts.h:509
@ CPSW_CPTS_IOCTL_SET_TS_NUDGE
CPTS set timestamp nudge.
Definition: cpsw_cpts.h:150
uint32_t seqId
Definition: cpsw_cpts.h:402