This is a flash-writer application which works in conjunction with the uart_uniflash.py python script mentioned in Flashing Tools. Although it is not strictly not a bootloader, it uses bootloader APIs to do basic SOC initialization required to be able to flash binaries to the OSPI flash. Like other SBLs, this is also booted by the ROM bootloader.
Once the example starts running it attempts to receive files via UART+XMODEM and process them in a loop. Once it receives a file (this is sent by the uart_uniflash.py script), it finds out what to do with the received file from the file header. It can be three things:
The meta-data required for doing these operations (offset, file size, erase size etc.) will be extracted from the same header.
After the file is processed, an acknowledgment is sent back to the host side python script and the loop continues.
This example is more or less like a flashing server, and will never terminate until EVM is powered down or the core is reset.
Parameter | Value |
---|---|
CPU + OS | r5fss0-0 nortos |
Toolchain | ti-arm-clang |
Boards | am243x-evm, am243x-lp |
Example folder | examples/drivers/boot/sbl_uart_uniflash |
Since this is mainly a flash-writer application, this is sent via the UART unlike other examples which are usually loaded with CCS. Nevertheless, you can build this example like you do for the others using makefile or build it via CCS by importing as a project.
Since this SBL receives the appimage and other files over UART using XMODEM protocol, it doesn't print anything to the console so as not to corrupt the XMODEM transport.