AM243x MCU+ SDK  08.02.00
I2C Led Blink

Introduction

This example demonstrates setting of multiple LED at the same time connected to the same I2C controller. The application will blink all the I2C controlled LED in the EVM.

Application exits after 10 iterations..

Supported Combinations

Parameter Value
CPU + OS r5fss0-0 freertos
r5fss0-0 nortos
Toolchain ti-arm-clang
Boards am243x-evm, am243x-lp
Example folder examples/drivers/i2c/i2c_led_blink

Steps to Run the Example

See Also

I2C

Sample Output

Shown below is a sample output when the application is run,

I2C LED Blink Test Started ...
LED will Blink for 10 loop ...
I2C LED Blink Test Passed!!
All tests have passed!!