PROFINET Device  v1.04.02
API Reference
Categories
[detail level 123]
 PROFINET API
 Physical Device API
 Physical Device Error Codes
 Ethernet Interface API
 Ethernet Interface Error Codes
 Simple Network Management Protocol
 Simple Network Management Protocol Error Codes
 PROFINET Device API
 PROFINET Device Error Codes
 Identification & Maintenance API
 Identification & Maintenance Error Codes
 PROFINET Library Configuration, Limits and SettingsPROFINET Library is been provided in different configurations in order to reduce the overhead of occupied and not used memory allocated by default. The Configuartion and Limits set you can read back here as a reference