PROFINET Device  v1.04.02

◆ PN_API_SNMP_applyPermanentData()

uint32_t PN_API_SNMP_applyPermanentData ( const PN_API_SNMP_SPermanentData_t pData_p)

Initialize a PDEV node.

ToDo.

Remarks
ToTo or remove tag.
Parameters
[in]adpPointer to the adapter.
[out]adpStatusPointer of type ei_api_adp_mod_net_status_t to the adapter status structure.
Returns
#PN_API_SNMP_error_t as uint32_t
Return values
#PN_API_SNMP_OK
Example
#include <PN_API_SNMP.h>
See also
PN_API_PDEV_start PN_API_PDEV_run