PROFINET Device  v1.04.02

◆ PN_API_DEV_setAlarm()

uint32_t PN_API_DEV_setAlarm ( uint16_t  alarmType_p)

Set IO device alarm.

ToDo.

Parameters
[in]alarmType_pAlarm type.
Returns
PN_API_DEV_EError_t as uint32_t
Return values
PN_API_DEV_eOK
Example
#include <PN_API_DEV.h>
See also
PN_API_PDEV_start PN_API_PDEV_run