Software installation
- Install a Code Composer Studio for Sitara(TM) processors (CCS).
- Install a System Configuration Tool (sysconfig).
- Install an ArmĀ® code generation tools - compiler (ARM-CGT)
- Install a Software Development Kit (SDK) AM243X with demos and device description ESI files
for details see Getting started
Connect the development board
TMDS243GPEVM/TMDS64GPEVM
Board details: TMDS64GPEVM, TMDS243GPEVM
Setup a dip switches on the board : 25MHz, No-boot / Dev-boot.
No boot mode
Connect the evaluation board to your computer using the micro-USB cables.
One USB cables is required for the JTAG interface (XDS110), a second cable for the UART console.
USB connectors on the AM64x/AM243 GP EVM Board
Connect an ethernet cable from a PC running the TwinCAT to EtherCAT IN/Port0 of the PRU-ICSS on the development board.
EtherCAT ports
- If you have multiple devices in chain, please connect from EtherCAT OUT/Port1 to IN/Port0 of next device. For the last device in chain, OUT/Port1 will be left open (if NOT using redundancy mode).
- Connect the board(s) to the power supply(ies) according to the specifications in the AM64x/AM243x GP EVM User's Guide Rev D
LP-AM243
Board details: LP-AM243
Setup a dip switches on the board : No-boot / Dev-boot
No boot mode
Connect the evaluation board to your computer using the micro-USB cable.
On the LP bards over the USB cable are connected the JTAG interface (XDS110) and the UART console.
USB connector on the AM243x LP Board
Connect an ethernet cable from a PC running the TwinCAT to EtherCAT IN/Port0 of the PRU-ICSS on the development board.
EtherCAT connectors on the AM243x LP Board
- If you have multiple devices in chain, please connect from EtherCAT OUT/Port1 to IN/Port0 of next device. For the last device in chain, OUT/Port1 will be left open (if NOT using redundancy mode).
Connect a USB Type-C Power Supply to the board
Board power connector on the AM243x LP
Steps to Run the Example
- When using CCS project to build, import the CCS project for the required combination and build it using the CCS project menu, see Using SDK with CCS Projects.
- When using makefiles to build, note the required combination and build using make command, see Using SDK with Makefiles.
- Lauch a CCS debug session and run the executable, seeCCS Lauch, Load and Run.