![Logo](ti_logo.svg) |
AM243x MCU+ SDK
08.01.00
|
|
Go to the documentation of this file.
53 #ifndef TISCI_PM_TISCI_DEVICE_H
54 #define TISCI_PM_TISCI_DEVICE_H
62 #define TISCI_MSG_FLAG_DEVICE_WAKE_ENABLED TISCI_BIT(8)
65 #define TISCI_MSG_FLAG_DEVICE_RESET_ISO TISCI_BIT(9)
74 #define TISCI_MSG_FLAG_DEVICE_EXCLUSIVE TISCI_BIT(10)
81 #define TISCI_MSG_VALUE_DEVICE_SW_STATE_AUTO_OFF 0
84 #define TISCI_MSG_VALUE_DEVICE_SW_STATE_RETENTION 1
87 #define TISCI_MSG_VALUE_DEVICE_SW_STATE_ON 2
93 #define TISCI_MSG_VALUE_DEVICE_HW_STATE_OFF 0
99 #define TISCI_MSG_VALUE_DEVICE_HW_STATE_ON 1
109 #define TISCI_MSG_VALUE_DEVICE_HW_STATE_TRANS 2
struct tisci_header hdr
Definition: tisci_pm_device.h:157
Empty response for TISCI_MSG_SET_DEVICE_RESETS.
Definition: tisci_pm_device.h:216
struct tisci_header hdr
Definition: tisci_pm_device.h:181
Request to get device based on id.
Definition: tisci_pm_device.h:156
uint32_t context_loss_count
Definition: tisci_pm_device.h:182
Empty response for TISCI_MSG_DEVICE_DROP_POWERUP_REF.
Definition: tisci_pm_device.h:245
uint8_t state
Definition: tisci_pm_device.h:133
struct tisci_header hdr
Definition: tisci_pm_device.h:130
struct tisci_header hdr
Definition: tisci_pm_device.h:217
Response to get device request.
Definition: tisci_pm_device.h:180
Empty response for TISCI_MSG_SET_DEVICE.
Definition: tisci_pm_device.h:144
Set the desired state of the device.
Definition: tisci_pm_device.h:129
struct tisci_header hdr
Definition: tisci_pm_device.h:246
Drop any remaining powerup device references.
Definition: tisci_pm_device.h:233
uint32_t reserved
Definition: tisci_pm_device.h:132
uint8_t programmed_state
Definition: tisci_pm_device.h:184
uint8_t current_state
Definition: tisci_pm_device.h:185
struct tisci_header hdr
Definition: tisci_pm_device.h:234
uint32_t id
Definition: tisci_pm_device.h:204
uint32_t resets
Definition: tisci_pm_device.h:205
struct tisci_header hdr
Definition: tisci_pm_device.h:203
uint32_t id
Definition: tisci_pm_device.h:131
uint32_t id
Definition: tisci_pm_device.h:158
struct tisci_msg_set_device_req __attribute__((__packed__))
uint32_t resets
Definition: tisci_pm_device.h:183
struct tisci_header hdr
Definition: tisci_pm_device.h:145
Set the desired state of the resets of a device.
Definition: tisci_pm_device.h:202