The following sections describe the steps to configure projects that contains one PLC that implementing EtherNet/IP Scanner functionality and one SITARA AM24x based EtherNet/IP Adapter device.
Examples are provided for a CODESYS IEC 61131 developments and runtime environments executing on an industrial RevPi Connect hardware (https://revolution.kunbus.com/) by KUNBUS GmbH and an Allen-Bradley CompactLogix L16ER PLC that is configured and programmed from the RSLogix 5000 development environment.
See Connecting the EtherNet/IP Adapter Example to a CODESYS based Controller
See Connecting the EtherNet/IP Adapter Example to an Allen-Bradley Controller