for details see Getting started
Board details: TMDS64GPEVM, TMDS243GPEVM
Setup a dip switches on the board : 25MHz, No-boot / Dev-boot.
Connect the evaluation board to your computer using the micro-USB cables.
One USB cables is required for the JTAG interface (XDS110), a second cable for the UART console.
Connect an ethernet cable from a PC running the TwinCAT to EtherCAT IN/Port0 of the PRU-ICSS on the development board.
Board details: LP-AM243
Setup a dip switches on the board : No-boot / Dev-boot
Connect the evaluation board to your computer using the micro-USB cable.
On the LP bards over the USB cable are connected the JTAG interface (XDS110) and the UART console.
Connect an ethernet cable from a PC running the TwinCAT to EtherCAT IN/Port0 of the PRU-ICSS on the development board.
Connect a USB Type-C Power Supply to the board
In the following instructions it is assumed the board LP_AM243. For other boards please choose always the right SDK and the example for your board.
Select a directory with your installed SDK, e.g.: C:\ti\YOUR_SDK_VERSION_DIRECTORY\examples\industrial_comms\ethercat_slave_demo
In the Console shall be show a message **** Build Finished ****
In the new opened window right click on Projects->ethercat_slave...->targetConfigs->AM....ccxml
WARNING: This is not the LP board!!!
A debug window will open.
In the Scripting Console type :
loadJSFile "C:\ti\YOUR_SDK_VERSION_DIRECTORY\tools\ccs_load\am64x_am243x\load_dmsc.js"
In the menu select Run->Load->Load program
Select a program and click OK.
Setup the terminal :
And start the terminal.
The application is running, a next step is to connect a PLC.