Macros | |
#define | DEFTYPE_NULL 0x0000 |
Null. More... | |
#define | DEFTYPE_BOOLEAN 0x0001 |
BOOLEAN. More... | |
#define | DEFTYPE_INTEGER8 0x0002 |
INTEGER8. More... | |
#define | DEFTYPE_INTEGER16 0x0003 |
INTEGER16. More... | |
#define | DEFTYPE_INTEGER32 0x0004 |
INTEGER32. More... | |
#define | DEFTYPE_UNSIGNED8 0x0005 |
UNSIGNED8. More... | |
#define | DEFTYPE_UNSIGNED16 0x0006 |
UNSIGNED16. More... | |
#define | DEFTYPE_UNSIGNED32 0x0007 |
UNSIGNED32. More... | |
#define | DEFTYPE_REAL32 0x0008 |
REAL32. More... | |
#define | DEFTYPE_VISIBLESTRING 0x0009 |
VISIBLE_STRING. More... | |
#define | DEFTYPE_OCTETSTRING 0x000A |
OCTET_STRING. More... | |
#define | DEFTYPE_UNICODE_STRING 0x000B |
UNICODE_STRING. More... | |
#define | DEFTYPE_TIME_OF_DAY 0x000C |
TIME_OF_DAY. More... | |
#define | DEFTYPE_TIME_DIFFERENCE 0x000D |
TIME_DIFFERENCE. More... | |
#define | DEFTYPE_INTEGER24 0x0010 |
INTEGER24. More... | |
#define | DEFTYPE_REAL64 0x0011 |
REAL64. More... | |
#define | DEFTYPE_INTEGER40 0x0012 |
INTEGER40. More... | |
#define | DEFTYPE_INTEGER48 0x0013 |
INTEGER48. More... | |
#define | DEFTYPE_INTEGER56 0x0014 |
INTEGER56. More... | |
#define | DEFTYPE_INTEGER64 0x0015 |
INTEGER64. More... | |
#define | DEFTYPE_UNSIGNED24 0x0016 |
UNSIGNED24. More... | |
#define | DEFTYPE_UNSIGNED40 0x0018 |
UNSIGNED40. More... | |
#define | DEFTYPE_UNSIGNED48 0x0019 |
UNSIGNED48. More... | |
#define | DEFTYPE_UNSIGNED56 0x001A |
UNSIGNED56. More... | |
#define | DEFTYPE_UNSIGNED64 0x001B |
UNSIGNED64. More... | |
#define | DEFTYPE_GUID 0x001D |
DEFTYPE_GUID. More... | |
#define | DEFTYPE_BYTE 0x001E |
DEFTYPE_BYTE. More... | |
#define | DEFTYPE_WORD 0x001F |
DEFTYPE_WORD. More... | |
#define | DEFTYPE_DWORD 0x0020 |
DEFTYPE_DWORD. More... | |
#define | DEFTYPE_PDOMAPPING 0x0021 |
PDO_MAPPING. More... | |
#define | DEFTYPE_IDENTITY 0x0023 |
IDENTITY. More... | |
#define | DEFTYPE_COMMAND 0x0025 |
COMMAND_PAR. More... | |
#define | DEFTYPE_PDOCOMPAR 0x0027 |
PDO_PARAMETER. More... | |
#define | DEFTYPE_ENUM 0x0028 |
DEFTYPE_ENUM. More... | |
#define | DEFTYPE_SMPAR 0x0029 |
SM_SYNCHRONISATION. More... | |
#define | DEFTYPE_RECORD 0x002A |
DEFTYPE_RECORD. More... | |
#define | DEFTYPE_BACKUP 0x002B |
BACKUP_PARAMETER. More... | |
#define | DEFTYPE_MDP 0x002C |
MODULAR_DEVICE_PROFILE. More... | |
#define | DEFTYPE_BITARR8 0x002D |
BITARR8. More... | |
#define | DEFTYPE_BITARR16 0x002E |
BITARR16. More... | |
#define | DEFTYPE_BITARR32 0x002F |
BITARR32. More... | |
#define | DEFTYPE_BIT1 0x0030 |
BIT1. More... | |
#define | DEFTYPE_BIT2 0x0031 |
BIT2. More... | |
#define | DEFTYPE_BIT3 0x0032 |
BIT3. More... | |
#define | DEFTYPE_BIT4 0x0033 |
BIT4. More... | |
#define | DEFTYPE_BIT5 0x0034 |
BIT5. More... | |
#define | DEFTYPE_BIT6 0x0035 |
BIT6. More... | |
#define | DEFTYPE_BIT7 0x0036 |
BIT7. More... | |
#define | DEFTYPE_BIT8 0x0037 |
BIT8. More... | |
#define | DEFTYPE_ARRAY_OF_INT 0x0260 |
DEFTYPE_ARRAY_OF_INT. More... | |
#define | DEFTYPE_ARRAY_OF_SINT 0x0261 |
DEFTYPE_ARRAY_OF_SINT. More... | |
#define | DEFTYPE_ARRAY_OF_DINT 0x0262 |
DEFTYPE_ARRAY_OF_DINT. More... | |
#define | DEFTYPE_ARRAY_OF_UDINT 0x0263 |
DEFTYPE_ARRAY_OF_UDINT. More... | |
#define | DEFTYPE_ERRORHANDLING 0x0281 |
DEFTYPE_ERRORHANDLING. More... | |
#define | DEFTYPE_DIAGHISTORY 0x0282 |
DEFTYPE_DIAGHISTORY. More... | |
#define | DEFTYPE_SYNCSTATUS 0x0283 |
DEFTYPE_SYNCSTATUS. More... | |
#define | DEFTYPE_SYNCSETTINGS 0x0284 |
DEFTYPE_SYNCSETTINGS. More... | |
#define | DEFTYPE_FSOEFRAME 0x0285 |
DEFTYPE_FSOEFRAME. More... | |
#define | DEFTYPE_FSOECOMMPAR 0x0286 |
DEFTYPE_FSOECOMMPAR. More... | |