uint32_t EC_API_SLV_CoE_configRecordSubIndex | ( | EC_API_SLV_SHandle_t * | pEcSlaveApi_p, |
EC_API_SLV_SCoE_Object_t * | pObject_p, | ||
uint8_t | subIndex_p, | ||
char * | pName_p, | ||
uint16_t | type_p, | ||
uint16_t | bitLen_p, | ||
uint16_t | flags_p | ||
) |
This function creates a subIndex for the Record Object.
[in] | pEcSlaveApi_p | The pointer to the EtherCAT API instance. |
[in] | pObject_p | Pointer to object instance. |
[in] | subIndex_p | Record subIndex. |
[in] | pName_p | Entry name. |
[in] | type_p | Entry data type. |
[in] | bitLen_p | Entry bit length. |
[in] | flags_p | Entry flags. |