Used to register process data buffer. Useful when the user wants to use its own buffers. If not used, then input and output buffers are allocated internally.
Functions | |
void | EC_API_SLV_cbRegisterPreSeqInputPDBuffer (EC_API_SLV_SHandle_t *pEcSlaveApi_p, void *pContext_p, EC_API_SLV_CBPreSeqInputPD_t cbFunc_p) |
This is the function to register a function which gets an external Process data buffer. More... | |
void | EC_API_SLV_cbRegisterPreSeqOutputPDBuffer (EC_API_SLV_SHandle_t *pEcSlaveApi_p, void *pContext_p, EC_API_SLV_CBPreSeqOutputPD_t cbFunc_p) |
This is the function to register a function which gets an external Process data buffer. More... | |
void | EC_API_SLV_cbRegisterPostSeqInputPDBuffer (EC_API_SLV_SHandle_t *pEcSlaveApi_p, void *pContext_p, EC_API_SLV_CBPostSeqInputPD_t cbFunc_p) |
This is the function to register a function which releases an external Process data buffer. More... | |
void | EC_API_SLV_cbRegisterPostSeqOutputPDBuffer (EC_API_SLV_SHandle_t *pEcSlaveApi_p, void *pContext_p, EC_API_SLV_CBPostSeqOutputPD_t cbFunc_p) |
This is the function to register a function which releases an external Process data buffer. More... | |