typedef int16_t(* EC_API_SLV_CBExtPhyLibDetect_t) (void *pPhyLibCtxt_p, uint8_t phyIdx_p, uint32_t phyId_p,uint8_t phyAddr_p, EC_API_SLV_SPhyDescriptor_t *pPhyLibDesc_p) |
Phy Detection callback of external PhyLib.
[in] | pPhyLibCtxt_p | External PhyLib Context |
[in] | phyIdx_p | Phy Instance (0/1) |
[in] | phyId_p | Phy ID read from hardware |
[in] | phyAddr_p | Phy address |
[in] | pPhyLibDesc_p | External PhyLib Hooks |