![Logo](ti_logo.svg) |
AM243x MCU+ SDK
08.01.00
|
|
Go to the documentation of this file.
71 #define ETHPHY_CMD_ENABLE_MII (0U)
75 #define ETHPHY_CMD_SOFT_RESTART (1U)
77 #define ETHPHY_CMD_ENABLE_AUTO_MDIX (2U)
81 #define ETHPHY_CMD_VERIFY_IDENTIFIER_REGISTER (3U)
83 #define ETHPHY_CMD_DISABLE_1000M_ADVERTISEMENT (4U)
89 #define ETHPHY_CMD_ENABLE_FAST_LINK_DOWN_DETECTION (5U)
95 #define ETHPHY_CMD_CONFIGURE_LED_SOURCE (6U)
101 #define ETHPHY_CMD_CONFIGURE_LED_BLINK_RATE (7U)
103 #define ETHPHY_CMD_ENABLE_EXTENDED_FD_ABILITY (8U)
105 #define ETHPHY_CMD_ENABLE_ODD_NIBBLE_DETECTION (9U)
107 #define ETHPHY_CMD_ENABLE_ENHANCED_IPG_DETECTION (10U)
109 #define ETHPHY_CMD_GET_LINK_STATUS (11U)
114 #define ETHPHY_CMD_GET_SPEED_AND_DUPLEX_CONFIG (12U)
119 #define ETHPHY_CMD_SET_SPEED_AND_DUPLEX_CONFIG (13U)
121 #define ETHPHY_CMD_ENABLE_LOW_LATENCY_10M_100M_RGMII (14U)
127 #define ETHPHY_CMD_SET_RX_HALF_FULL_THRESHOLD_RGMII (15U)
133 #define ETHPHY_CMD_SET_TX_HALF_FULL_THRESHOLD_RGMII (16U)
140 #define ETHPHY_CMD_GET_AUTONEG_COMPLETE_STATUS (17U)
147 #define ETHPHY_CMD_GET_LINK_PARTNER_AUTONEG_ABILITY (18U)
158 #define ETHPHY_SPEED_DUPLEX_CONFIG_AUTONEG (0U)
159 #define ETHPHY_SPEED_DUPLEX_CONFIG_10FD (1U)
160 #define ETHPHY_SPEED_DUPLEX_CONFIG_100FD (2U)
161 #define ETHPHY_SPEED_DUPLEX_CONFIG_1000FD (3U)
162 #define ETHPHY_SPEED_DUPLEX_CONFIG_10HD (4U)
163 #define ETHPHY_SPEED_DUPLEX_CONFIG_100HD (5U)
164 #define ETHPHY_SPEED_DUPLEX_CONFIG_1000HD (6U)
165 #define ETHPHY_SPEED_DUPLEX_CONFIG_INVALID (7U)
234 typedef struct ETHPHY_Params_s
242 typedef struct ETHPHY_Fxns_s
253 typedef struct ETHPHY_Attrs_s
263 typedef struct ETHPHY_Config_s
275 typedef struct ETHPHY_SpeedDuplexConfig_s
284 #include <board/ethphy/ethphy_dp83869.h>
struct ETHPHY_Params_s ETHPHY_Params
Forward declaration of ETHPHY_Params.
Definition: ethphy.h:173
uint32_t phyAddress
Definition: ethphy.h:256
const ETHPHY_Attrs * ETHPHY_getAttrs(uint32_t instanceId)
Return ETHPHY attributes.
Data structure to be passed/returned when calling ETHPHY_command with ETHPHY_CMD_GET_SPEED_AND_DUPLEX...
Definition: ethphy.h:276
int32_t(* ETHPHY_OpenFxn)(ETHPHY_Config *config, const ETHPHY_Params *params)
Driver implementation to open a specific ETHPHY driver.
Definition: ethphy.h:192
ETHPHY_Attrs * attrs
Definition: ethphy.h:265
uint32_t mdioBaseAddress
Definition: ethphy.h:255
uint32_t data
Definition: tisci_rm_psil.h:1
Parameters passed during ETHPHY_open()
Definition: ethphy.h:235
void * object
Definition: ethphy.h:267
uint32_t config
Definition: ethphy.h:277
void ETHPHY_close(ETHPHY_Handle handle)
Close ETHPHY driver.
ETHPHY_CommandFxn commandFxn
Definition: ethphy.h:246
ETHPHY_CloseFxn closeFxn
Definition: ethphy.h:245
int32_t(* ETHPHY_CommandFxn)(ETHPHY_Config *config, uint32_t command, void *data, uint32_t dataSize)
Driver implementation to send command to the ETHPHY using specific ETHPHY driver.
Definition: ethphy.h:220
void ETHPHY_Params_init(ETHPHY_Params *params)
Set default parameters in the ETHPHY_Params structure.
ETHPHY device attributes. These are filled by SysCfg based on the PHY device that is selected.
Definition: ethphy.h:254
ETHPHY Driver implementation callbacks.
Definition: ethphy.h:243
ETHPHY driver configuration. These are filled by SysCfg based on the PHY device that is selected.
Definition: ethphy.h:264
struct ETHPHY_Config_s ETHPHY_Config
Forward declaration of ETHPHY_Config.
Definition: ethphy.h:171
ETHPHY_OpenFxn openFxn
Definition: ethphy.h:244
ETHPHY_Handle ETHPHY_open(uint32_t instanceId, const ETHPHY_Params *params)
Open ETHPHY driver.
ETHPHY_Fxns * fxns
Definition: ethphy.h:266
int32_t ETHPHY_command(ETHPHY_Handle handle, uint32_t command, void *data, uint32_t dataSize)
Send a command to the ETHPHY.
void * ETHPHY_Handle
Handle to the ETHPHY driver returned by ETHPHY_open()
Definition: ethphy.h:169
uint32_t reserved
Definition: ethphy.h:236
void(* ETHPHY_CloseFxn)(ETHPHY_Config *config)
Driver implementation to close a specific ETHPHY driver.
Definition: ethphy.h:204