The Ethernet Link Object maintains link-specific counters and status information for an IEEE 802.3 communications interface. Each device supports exactly one instance of the Ethernet Link Object for each communications interface on the module.
| Attribute ID | Access Rule | NV | Name | Data Type | Value | Description | |
|---|---|---|---|---|---|---|---|
| 3 | Get, Set ¹ | NV | Physical Address | ARRAY of 6 USINTs | <MAC layer address> | The Physical Address attribute contains the interface's MAC layer address. The Physical address is an array of octets. The recommended display format is XX-XX-XX-XX-XX-XX, starting with the first octet.
| |
| 6 | Get ², Set | NV | Interface Control | STRUCT of: | Bit | Content | Configuration for physical interface |
| Control Bits | UINT | 0: | 0/1 | Auto-negotiate
| |||
| 1: | 0/1 | Forced Duplex Mode Auto-negotiate bit = 0: The forced Duplex Mode bit indicates whether the interface shall operate in full or half duplex mode.
Auto-negotiate bit = 1: If auto-negotiation is enabled, attempting to set the Forced Duplex Mode bit shall result in status code 0x0C (Object State Conflict). | |||||
| 2..15: | 0 | reserved Shall be set to 0. | |||||
| Forced Interface Speed | WORD | <speed value> | Speed in Mbps (10, 100, 1000, etc.) | ||||
Table Footnotes:
¹ Set access only with application's Set function
² Get access only with application's Get function
Functions | |
| uint32_t | EI_API_ADP_getMacAddr (T *pAdp_p, EI_API_ADP_SParam_t *pMacAddr_p) |
| Get the adapter MAC address (Instance Attribute ID: 3). More... | |
| uint32_t | EI_API_ADP_getIntfConfig (T *pAdp_p, uint8_t intfId_p, EI_API_ADP_UIntfConf_t *pIntfConf_p) |
| Get the current adapter configuration of interface with the specified ID (Instance Attribute ID: 6). More... | |
| uint32_t | EI_API_ADP_setIntfConfig (T *adp, uint8_t intfId, EI_API_ADP_UIntfConf_t intfConfig) |
| Set the adapter Ethernet interface configuration (Instance Attribute ID: 6). More... | |