EtherCAT Slave  1.04.01

◆ EC_API_SLV_CBPhySpecific_SoftReset_t

typedef void(* EC_API_SLV_CBPhySpecific_SoftReset_t) (void *pAppContext_p, void *pStackContext_p, uint32_t phyAddr_p)

Issue PHY Reset by software (used if no Hard Reset is available)

Parameters
[in]pAppContext_papplication context
[in]pStackContext_pslave stack context
[in]phyAddr_pphy address