EtherCAT Slave  1.04.01

◆ EC_API_SLV_CBPhySpecific_rgmiiRxHalfFullThreshold_t

typedef void(* EC_API_SLV_CBPhySpecific_rgmiiRxHalfFullThreshold_t) (void *pAppContext_p, void *pStackContext_p, uint32_t phyAddr_p, uint32_t threshold_p)

RGMII_RX_HALF_FULL_THR[1:0] can be changed from the default of 0x2 to 0x1. This will reduce the latency by one clock period.

Parameters
[in]pAppContext_papplication context
[in]pStackContext_pslave stack context
[in]phyAddr_pphy address
[in]threshold_pNumber of cycles for threshold (2, 1)