![Logo](ti_logo.svg) |
AM243x MCU+ SDK
08.00.00
|
|
Go to the documentation of this file.
54 #ifndef RM_TISCI_IRQ_H
55 #define RM_TISCI_IRQ_H
62 #define TISCI_MSG_VALUE_RM_DST_ID_VALID (1u << 0u)
67 #define TISCI_MSG_VALUE_RM_DST_HOST_IRQ_VALID (1u << 1u)
72 #define TISCI_MSG_VALUE_RM_IA_ID_VALID (1u << 2u)
77 #define TISCI_MSG_VALUE_RM_VINT_VALID (1u << 3u)
82 #define TISCI_MSG_VALUE_RM_GLOBAL_EVENT_VALID (1u << 4u)
87 #define TISCI_MSG_VALUE_RM_VINT_STATUS_BIT_INDEX_VALID (1u << 5u)
uint16_t src_index
Definition: tisci_rm_irq.h:196
uint16_t dst_host_irq
Definition: tisci_rm_irq.h:324
uint16_t vint
Definition: tisci_rm_irq.h:326
uint16_t dst_id
Definition: tisci_rm_irq.h:323
uint32_t valid_params
Definition: tisci_rm_irq.h:320
uint16_t dst_host_irq
Definition: tisci_rm_irq.h:198
uint16_t global_event
Definition: tisci_rm_irq.h:327
uint16_t src_id
Definition: tisci_rm_irq.h:195
Configures peripherals within the interrupt subsystem according to the valid configuration provided....
Definition: tisci_rm_irq.h:192
uint8_t vint_status_bit_index
Definition: tisci_rm_irq.h:202
uint16_t dst_id
Definition: tisci_rm_irq.h:197
uint16_t global_event
Definition: tisci_rm_irq.h:201
struct tisci_header hdr
Definition: tisci_rm_irq.h:193
uint16_t vint
Definition: tisci_rm_irq.h:200
struct tisci_header hdr
Definition: tisci_rm_irq.h:213
uint16_t src_index
Definition: tisci_rm_irq.h:322
struct tisci_header hdr
Definition: tisci_rm_irq.h:339
uint32_t valid_params
Definition: tisci_rm_irq.h:194
struct tisci_msg_rm_irq_set_req __attribute__((__packed__))
uint16_t ia_id
Definition: tisci_rm_irq.h:199
Response to setting a peripheral to processor interrupt.
Definition: tisci_rm_irq.h:212
uint16_t ia_id
Definition: tisci_rm_irq.h:325
uint8_t secondary_host
Definition: tisci_rm_irq.h:203
uint8_t secondary_host
Definition: tisci_rm_irq.h:329
struct tisci_header hdr
Definition: tisci_rm_irq.h:319
Response to releasing a peripheral to processor interrupt.
Definition: tisci_rm_irq.h:338
Releases interrupt peripheral resources according to the valid configuration provided....
Definition: tisci_rm_irq.h:318
uint16_t src_id
Definition: tisci_rm_irq.h:321
uint8_t vint_status_bit_index
Definition: tisci_rm_irq.h:328