![Logo](ti_logo.svg) |
AM243x MCU+ SDK
08.00.00
|
|
Go to the documentation of this file.
90 #ifndef DISABLE_UART_PRINT
94 #include <industrial_protocols/ethercat_slave/icss_fwhal/tiesc_pruss_intc_mapping.h>
96 #include <industrial_protocols/ethercat_slave/icss_fwhal/tiesc_def.h>
111 #define ENABLE_MULTIPLE_SM_ACCESS_IN_SINGLE_DATAGRAM 0
113 #define MAX_SYNC_MAN 8
114 #define SIZEOF_SM_REGISTER 8
116 #define TIESC_EEPROM_SIZE 0x800
118 #define MAILBOX_WRITE 0
119 #define MAILBOX_READ 1
120 #define PROCESS_DATA_OUT 2
121 #define PROCESS_DATA_IN 3
123 #define MBX_WRITE_EVENT ((uint16_t) 0x0100)
124 #define MBX_READ_EVENT ((uint16_t) 0x0200)
127 #define ESC_ADDR_REV_TYPE 0x000
128 #define ESC_ADDR_BUILD 0x002
130 #define ESC_ADDR_CONFIG_STATION_ALIAS 0x012
131 #define ESC_ADDR_DLSTATUS 0x110
132 #define ESC_ADDR_ALCONTROL 0x120
133 #define ESC_ADDR_ALSTATUS 0x130
134 #define ESC_ADDR_PDI_CONTROL 0x140
135 #define ESC_PDI_CONTROL_ELD_ALL_PORTS_MASK (1 << 1)
136 #define ESC_ADDR_PDI_CONFIG 0x150
137 #define ESC_ADDR_AL_EVENT_MASK 0x204
138 #define ESC_ADDR_AL_EVENT_REQ 0x220
139 #define ESC_ADDR_SM_WD_STATUS 0x440
140 #define ESC_ADDR_EEPROM_CTRL 0x502
141 #define ESC_ADDR_MI_ECAT_ACCESS 0x516
142 #define ESC_ADDR_MI_PDI_ACCESS 0x517
144 #define ESC_EEPROM_CMD_MASK 0x0700 //Description (0x502.8:10): Command bit mask
145 #define ESC_EEPROM_CMD_READ_MASK 0x0100 //Description (0x502.8): Currently executed read command
146 #define ESC_EEPROM_CMD_WRITE_MASK 0x0200 //Description (0x502.9): Initialize Write Command
147 #define ESC_EEPROM_CMD_RELOAD_MASK 0x0400 //Description (0x502.10): Trigger EEPROM reload
148 #define ESC_EEPROM_ERROR_MASK 0x7800 //Description : Mask all EEPROM error bits; Checksum error (0x0502.11); EEPROM not loaded (0x0502.12); Missing EEPROM Acknowledge (0x0502.13); Write Error (0x0502.14)
149 #define ESC_EEPROM_ERROR_CRC 0x0800 //Description (0x502.11): EEPROM CRC Error
150 #define ESC_EEPROM_ERROR_CMD_ACK 0x2000 //Description (0x502.13): EEPROM Busy
151 #define ESC_EEPROM_BUSY_MASK 0x8000 //Description (0x502.15): EEPROM Busy
153 #define ESC_ADDR_SYNCMAN 0x800
155 #define ESC_ADDR_SM1_STATUS 0x80D
156 #define SM_STATUS_MBX_FULL 0x08
158 #define ESC_ADDR_SM0_STATUS 0x805
159 #define ESC_ADDR_SM0_ACTIVATE 0x806
160 #define ESC_ADDR_SM1_ACTIVATE 0x806+8
161 #define ESC_ADDR_SM2_ACTIVATE 0x806+8*2
162 #define ESC_ADDR_SM3_ACTIVATE 0x806+8*3
163 #define ESC_ADDR_SM4_ACTIVATE 0x806+8*4
164 #define ESC_ADDR_SM5_ACTIVATE 0x806+8*5
165 #define ESC_ADDR_SM6_ACTIVATE 0x806+8*6
166 #define ESC_ADDR_SM7_ACTIVATE 0x806+8*7
167 #define ESC_ADDR_SM0_PDI_CONTROL 0x807
168 #define ESC_ADDR_SM1_PDI_CONTROL 0x807+8
169 #define ESC_ADDR_SM2_PDI_CONTROL 0x807+8*2
170 #define ESC_ADDR_SM3_PDI_CONTROL 0x807+8*3
171 #define ESC_ADDR_SM4_PDI_CONTROL 0x807+8*4
172 #define ESC_ADDR_SM5_PDI_CONTROL 0x807+8*5
173 #define ESC_ADDR_SM6_PDI_CONTROL 0x807+8*6
174 #define ESC_ADDR_SM7_PDI_CONTROL 0x807+8*7
176 #define SM_PDI_CONTROL_SM_DISABLE 1
178 #define ESC_ADDR_SYSTIME 0x910
179 #define ESC_ADDR_SYSTIME_HIGH 0x914
180 #define ESC_ADDR_SYSTIME_OFFSET 0x920
181 #define ESC_ADDR_SYSTIME_DELAY 0x928
182 #define ESC_ADDR_SPEEDCOUNTER_START 0x930
183 #define ESC_ADDR_TIMEDIFF_FILTDEPTH 0x934
184 #define ESC_ADDR_SPEEDDIFF_FILTDEPTH 0x935
185 #define ESC_ADDR_SYNC_PULSE_LENGTH 0x982
186 #define ESC_ADDR_SYNC_STATUS 0x98E
187 #define ESC_ADDR_LATCH0_CONTROL 0x9A8
188 #define ESC_ADDR_LATCH1_CONTROL 0x9A9
189 #define ESC_ADDR_LATCH0_POS_EDGE 0x9B0
190 #define ESC_ADDR_LATCH0_NEG_EDGE 0x9B8
191 #define ESC_ADDR_LATCH1_POS_EDGE 0x9C0
192 #define ESC_ADDR_LATCH1_NEG_EDGE 0x9C8
193 #define ESC_ADDR_TI_PORT0_ACTIVITY 0xE00
194 #define ESC_ADDR_TI_PORT1_ACTIVITY 0xE04
195 #define ESC_ADDR_TI_PORT0_PHYADDR 0xE08
196 #define ESC_ADDR_TI_PORT1_PHYADDR 0xE09
197 #define ESC_ADDR_TI_PDI_ISR_PINSEL 0xE0A
198 #define ESC_ADDR_TI_PHY_LINK_POLARITY 0XE0C
199 #define ESC_ADDR_TI_PORT0_TX_START_DELAY 0xE10
200 #define ESC_ADDR_TI_PORT1_TX_START_DELAY 0xE12
201 #define ESC_ADDR_TI_ESC_RESET 0xE14
202 #define ESC_ADDR_TI_EDMA_LATENCY_ENHANCEMENT 0xE24
203 #define TI_ESC_RST_CMD_U 0x545352
204 #define TI_ESC_RST_CMD_L 0x747372
206 #define ESC_ADDR_MEMORY 0x1000
208 #define CMD_DL_USER_CLEAR_AL_EVENT_HIGH 0x0
209 #define CMD_DL_USER_GET_BUFFER_READ_ADDR 0x1
210 #define CMD_DL_USER_GET_BUFFER_WRITE_ADDR 0x2
211 #define CMD_DL_USER_SET_BUFFER_WRITE_DONE 0x3
216 #define CMD_DL_USER_ACK_MBX_READ 0x4
221 #define CMD_DL_USER_ACK_MBX_WRITE 0x5
226 #define CMD_DL_USER_EEPROM_CMD_ACK 0x6
231 #define CMD_DL_USER_READ_SYNC_STATUS 0x7
238 #define CMD_DL_USER_READ_AL_CONTROL 0x8
243 #define CMD_DL_USER_WRITE_AL_STATUS 0x9
248 #define CMD_DL_USER_READ_PD_WD_STATUS 0xA
253 #define CMD_DL_USER_READ_SM_ACTIVATE 0xB
258 #define CMD_DL_USER_WRITE_SM_PDI_CTRL 0xC
263 #define CMD_DL_USER_READ_LATCH_TIME 0xD
264 #define LATCH0_POS_EDGE 0
265 #define LATCH0_NEG_EDGE 1
266 #define LATCH1_POS_EDGE 2
267 #define LATCH1_NEG_EDGE 3
273 #define CMD_DL_USER_READ_SYS_TIME 0xE
278 #define CMD_DL_USER_CLEAR_AL_EVENT_LOW 0xF
279 #ifdef SYSTEM_TIME_PDI_CONTROLLED
284 #define CMD_DL_USER_SYSTIME_PDI_CONTROL 0x10
285 #define WRITE_SYSTIME 0
286 #define WRITE_SYSTIME_OFFSET 1
287 #define WRITE_FILTER_CONFIG 2
293 #define ICSS_MDIO_USRPHYSEL_LINKINT_ENABLE 0x40
294 #define ICSS_MDIO_USRPHYSEL_LINKSTAT_MLINK 0x80
296 #define TIESC_PERM_RW 0x0
297 #define TIESC_PERM_WRITE_ONLY 0x1
298 #define TIESC_PERM_READ_ONLY 0x2
300 #define TIESC_PERM_WRITE TIESC_PERM_WRITE_ONLY
301 #define TIESC_PERM_READ TIESC_PERM_READ_ONLY
303 #define PDI_PERM_RW 0x0
304 #define PDI_PERM_READ_ONLY 0x1
306 #define PDI_PERM_WRITE PDI_PERM_RW
307 #define PDI_PERM_READ PDI_PERM_READ_ONLY
309 #define TIESC_MDIO_CLKDIV 79 //For 2.5MHz MDIO clock: 200/(TIESC_MDIO_CLKDIV+1)
311 #define TIESC_MDIO_RX_LINK_DISABLE 0 //Slow MDIO state m/c based link detection
312 #define TIESC_MDIO_RX_LINK_ENABLE 1 //Fast link detect using RXLINK forward from PHY to MDIO MLINK
313 #define TIESC_LINK_POL_ACTIVE_LOW 1
314 #define TIESC_LINK_POL_ACTIVE_HIGH 0
320 #define PDI_WD_TRIGGER_RX_SOF (0 << 4)
326 #define PDI_WD_TRIGGER_LATCH_IN (1 << 4)
332 #define PDI_WD_TRIGGER_SYNC0_OUT (2 << 4)
338 #define PDI_WD_TRIGGER_SYNC1_OUT (3 << 4)
340 #if ENABLE_MULTIPLE_SM_ACCESS_IN_SINGLE_DATAGRAM
341 #define TIESC_PORT0_TX_DELAY 0x98
343 #define TIESC_PORT0_TX_DELAY 0x48
345 #define TIESC_PORT1_TX_DELAY TIESC_PORT0_TX_DELAY
347 #define PDI_ISR_EDIO_NUM 7 //GPMC_CSN(2) -> pr1_edio_data_out7 for ICEv2.J4.Pin21
353 #define USE_ECAT_TIMER
360 #define ENABLE_PDI_TASK
361 #define ENABLE_SYNC_TASK
371 #if defined (__aarch64__)
372 #define ASSERT_DMB() __asm__(" dmb ISH")
373 #define ASSERT_DSB() __asm__(" dsb ISH")
375 #define ASSERT_DMB() __asm__(" dmb")
376 #define ASSERT_DSB() __asm__(" dsb")
379 #ifdef USE_ECAT_TIMER
380 #define ECAT_TIMER_INC_P_MS 1000000
382 #define ECAT_TIMER_INC_P_MS ecat_timer_inc_p_ms
383 extern volatile uint32_t ecat_timer_inc_p_ms;
386 #define ESC_SYSTEMTIME_OFFSET_OFFSET 0x0920
387 #define ESC_SPEED_COUNTER_START_OFFSET 0x0930
388 #define ESC_DC_START_TIME_CYCLIC_OFFSET 0x0990
390 #define DRIFTCTRL_TASK_SYNC_ZERO_CROSS_ADJUST 0xE0 //PRU_DMEM0
396 #define LOCK_PD_BUF_AVAILABLE_FOR_HOST 0
401 #define LOCK_PD_BUF_HOST_ACCESS_START 1
406 #define LOCK_PD_BUF_HOST_ACCESS_FINISH 2
414 #define LOCK_PD_BUF_CHECK_AVAILABILITY_RETRY_COUNT (10U)
432 typedef struct bsp_params_s
493 uint8_t reserved1[0x90];
497 uint8_t reserved2[7];
504 #ifndef SYSTEM_TIME_PDI_CONTROLLED
505 uint8_t reserved3[212];
507 uint8_t reserved3[24];
508 uint32_t systime_offset_low;
509 uint32_t systime_offset_high;
510 uint8_t reserved4[180];
521 uint8_t reg_properties[4096];
683 uint32_t command, uint16_t param1, uint16_t param2);
710 int32_t reload_flag);
803 uint16_t address, uint16_t len);
890 uint16_t address, uint16_t len, int16_t *p_sm_index);
904 uint16_t address, uint16_t len, int16_t sm_index);
1013 uint16_t address, uint16_t length);
1029 uint16_t address, uint16_t length,
1074 uint16_t address, uint16_t len);
1085 uint32_t regoffset);
1096 uint32_t regoffset);
1107 uint32_t regoffset);
1118 uint32_t regoffset);
1261 uint8_t phyaddr, uint8_t regoffset, uint16_t *regval);
1274 uint8_t phyaddr, uint8_t regoffset, uint16_t regval);
1350 #ifdef SYSTEM_TIME_PDI_CONTROLLED
1358 extern void bsp_pdi_latch0_control(
PRUICSS_Handle pruIcssHandle, uint8_t val);
1367 extern void bsp_pdi_latch1_control(
PRUICSS_Handle pruIcssHandle, uint8_t val);
1375 extern void bsp_pdi_write_system_time(
PRUICSS_Handle pruIcssHandle,
1383 extern void bsp_pdi_write_system_timeoffset(
PRUICSS_Handle pruIcssHandle,
1384 unsigned long long systime);
1391 extern void bsp_pdi_write_systime_delay(
PRUICSS_Handle pruIcssHandle,
1401 extern void bsp_pdi_write_filterconfig(
PRUICSS_Handle pruIcssHandle,
1402 uint16_t speedcount_start,
1403 uint8_t speedcount_filtdepth, uint8_t systime_filtdepth);
1431 uint32_t *systime_high);
1441 uint32_t *systime_low, uint32_t *systime_high);
1451 uint32_t *systime_low, uint32_t *systime_high);
1461 uint32_t *systime_low, uint32_t *systime_high);
1471 uint32_t *systime_low, uint32_t *systime_high);
1510 #ifndef SUPPORT_CMDACK_POLL_MODE
1534 uint32_t *hostProc, uint32_t hostProcLen);
void bsp_set_eeprom_update_status(uint8_t status)
Indicate to FWHAL whether EEPROM is written for flushing to non-volatile storage. Typically called on...
uint32_t phy1_address
Definition: tiescbsp.h:462
uint8_t sm_buf_index
Definition: tiescbsp.h:482
uint32_t bsp_get_pdi_read_access_fail_cnt()
Returns the count of PDI read access failures.
uint32_t bsp_hwspinlock_lock(int num)
Acquire selected spinlock instance.
uint16_t resp2low
Definition: tiescbsp.h:503
void bsp_pdi_post_read_indication(PRUICSS_Handle pruIcssHandle, uint16_t address, uint16_t length)
Invoked after reading a register or mailbox buffer from PDI side .
void EscCmdLowAckIsr(void *args)
ESC CMD Low ACK IRQ Handler.
void bsp_eeprom_emulation_exit(void)
Call EEPROM flush on exit.
uint16_t size
Definition: tisci_boardcfg.h:1
void bsp_get_latch0_posedge_time(PRUICSS_Handle pruIcssHandle, uint32_t *systime_low, uint32_t *systime_high)
Return latch0 posedge timestamp for application use(nanosec resolution)
void bsp_pdi_mbx_write_start(PRUICSS_Handle pruIcssHandle)
Indicates to the firmware that PDI side write to read mailbox has started.
void bsp_global_mutex_lock(void)
Critical section enter API using semaphore/mutex/interrupt disable primitives from RTOS....
uint8_t bsp_pdi_access_perm_dword(uint16_t address, uint8_t access)
Checks if the PDI register [Four bytes] has the requested access permission and returns the result.
uint8_t ** eeprom_pointer_for_stack
Definition: tiescbsp.h:466
uint32_t system_time_low
Definition: tiescbsp.h:494
uint16_t cmdlow_ack
Definition: tiescbsp.h:499
Struct for host to PRU-ICSS command interface.
Definition: tiescbsp.h:481
uint8_t addr0
Definition: tiescbsp.h:536
void bsp_process_data_access_complete(PRUICSS_Handle pruIcssHandle, uint16_t address, uint16_t len, int16_t sm_index)
This API is invoked after PDI side completes read/write to PD address returned by bsp_get_process_dat...
bsp_ethphy_init_t ethphy_init
Definition: tiescbsp.h:451
uint16_t bsp_read_word(PRUICSS_Handle pruIcssHandle, uint16_t address)
Read a 16-bit value at 'Address' from ESC memory: SM mailbox (single buffer) mapped or register area.
uint8_t lock_state
Definition: tiescbsp.h:483
void bsp_get_latch1_posedge_time(PRUICSS_Handle pruIcssHandle, uint32_t *systime_low, uint32_t *systime_high)
Return latch1 posedge timestamp for application use(nanosec resolution)
void bsp_hwspinlock_unlock(int num)
Release selected spinlock instance.
uint8_t bsp_is_pdi_perm_read_only(uint16_t *perm_array, uint16_t address)
Checks if the PDI register [byte] has read only access permission and returns the result.
void bsp_send_command_to_firmware(PRUICSS_Handle pruIcssHandle, uint32_t command, uint16_t param1, uint16_t param2)
Send command and parameters from stack to firmware to perform some action based on stack state or in ...
uint8_t bsp_read_byte(PRUICSS_Handle pruIcssHandle, uint16_t address)
Read a byte value at 'Address' from ESC memory: SM mailbox (single buffer) mapped or register area.
void bsp_pdi_write_indication(PRUICSS_Handle pruIcssHandle, uint16_t address, uint16_t length, uint16_t value)
Invoked after writing a register or mailbox buffer from PDI side .
uint16_t length
Definition: tiescbsp.h:527
void bsp_params_init(bsp_params *init_params)
Initialize the members of bsp_params with default values.
Definition: tiescbsp.h:525
void bsp_pruss_iepreg_write(PRUICSS_Handle pruIcssHandle, uint32_t val, uint32_t regoffset)
Write a 32-bit value from PRU-ICSS IEP register at 'regoffset'.
uint32_t bsp_pruss_mdioreg_read(PRUICSS_Handle pruIcssHandle, uint32_t regoffset)
Read a 32-bit value from PRU-ICSS MDIO register at 'regoffset'.
void(* bsp_hwspinlock_unlock_t)(int num)
Definition: tiescbsp.h:420
uint32_t bsp_read_dword_isr(PRUICSS_Handle pruIcssHandle, uint16_t address)
Read a 32-bit value at 'Address' from ESC process data memory: SM buffer (3-buffer) mapped area.
int32_t bsp_eeprom_emulation_reload(PRUICSS_Handle pruIcssHandle)
Perform reload operation after validating EEPROM CRC.
void bsp_set_pdi_wd_trigger_mode(PRUICSS_Handle pruIcssHandle, uint32_t mode)
Configure PDI WD trigger mode, PDI WD is triggered automatically by h/w on RX_SOF(port0/port1),...
void bsp_eeprom_emulation_flush(void)
Flush the EEPROM cache to non-volatile storage. Write is performed using eeprom_write callback from b...
void bsp_read(PRUICSS_Handle pruIcssHandle, uint8_t *pdata, uint16_t address, uint16_t len)
Read a byte array at 'address' from ESC memory.
uint16_t bsp_get_process_data_address(PRUICSS_Handle pruIcssHandle, uint16_t address, uint16_t len, int16_t *p_sm_index)
Get the actual address of the buffer for PDI side read/write from host in 3-buffer mode.
int32_t(* bsp_eeprom_read_t)(uint8_t *buf, uint32_t len)
Definition: tiescbsp.h:416
uint16_t bsp_read_word_isr(PRUICSS_Handle pruIcssHandle, uint16_t address)
Read a 16-bit value at 'Address' from ESC process data memory: SM buffer (3-buffer) mapped area.
void bsp_set_sm_properties(PRUICSS_Handle pruIcssHandle, uint8_t sm, uint16_t address, uint16_t len)
Set the address, length info from register to FWHAL layer. During INIT to PREOP transition in Mailbox...
uint32_t system_time_high
Definition: tiescbsp.h:495
bsp_ethercat_stack_isr_function pdi_isr
Definition: tiescbsp.h:469
int16_t bsp_pruss_mdio_phy_write(PRUICSS_Handle pruIcssHandle, uint8_t phyaddr, uint8_t regoffset, uint16_t regval)
API to write PHY register via PRU-ICSS MDIO.
uint32_t spinlock_base_address
Definition: tiescbsp.h:448
Struct for register permission array.
Definition: tiescbsp.h:519
void bsp_get_latch1_negedge_time(PRUICSS_Handle pruIcssHandle, uint32_t *systime_low, uint32_t *systime_high)
Return latch0 negedge timestamp for application use(nanosec resolution)
void bsp_set_pru_firmware(uint32_t *frameProc, uint32_t frameProcLen, uint32_t *hostProc, uint32_t hostProcLen)
This function internally sets the location from which PRU firmwares can be loaded.
uint8_t bsp_pdi_access_perm_word(uint16_t address, uint8_t access)
Checks if the PDI register [Two bytes] has the requested access permission and returns the result.
void bsp_set_pdi_perm_read_only(uint16_t *perm_array, uint16_t address)
Set the PDI register [byte] access permission to read only.
void(* bsp_ethphy_init_t)(PRUICSS_Handle pruIcssHandle, uint8_t phy0addr, uint8_t phy1addr, uint8_t enhancedlink_enable)
Definition: tiescbsp.h:421
int32_t(* bsp_eeprom_write_t)(uint8_t *buf, uint32_t len)
Definition: tiescbsp.h:417
uint8_t enhancedlink_enable
Definition: tiescbsp.h:540
uint32_t value
Definition: tisci_otp_revision.h:2
void bsp_set_eeprom_updated_time(void)
Set EEPROM update time.
void bsp_write_byte(PRUICSS_Handle pruIcssHandle, uint8_t val, uint16_t address)
Write a byte value at 'address' in ESC memory.
int32_t bsp_eeprom_load_esc_registers(PRUICSS_Handle pruIcssHandle, int32_t reload_flag)
For loading ESC registers from EEPROM during first boot/reload after validating CRC.
void bsp_esc_reg_perm_init(PRUICSS_Handle pruIcssHandle)
Sets up register permissions for ECAT side access for TI ESC, if ENABLE_PDI_REG_PERMISSIONS is define...
void bsp_write(PRUICSS_Handle pruIcssHandle, uint8_t *pdata, uint16_t address, uint16_t len)
Write 'len' bytes from pdata to 'address' in ESC memory.
uint8_t addr1
Definition: tiescbsp.h:537
uint16_t resp1low
Definition: tiescbsp.h:502
void bsp_write_word(PRUICSS_Handle pruIcssHandle, uint16_t val, uint16_t address)
Write a 16-bit value at 'address' in ESC memory.
void(* bsp_init_spinlock_t)(void)
Definition: tiescbsp.h:418
void bsp_eeprom_emulation_command_ack(PRUICSS_Handle pruIcssHandle)
Perform reload operation after validating EEPROM CRC, Wrapper API for SSC.
int16_t bsp_pruss_mdio_phy_read(PRUICSS_Handle pruIcssHandle, uint8_t phyaddr, uint8_t regoffset, uint16_t *regval)
API to read PHY register via PRU-ICSS MDIO.
uint8_t link1pol
Definition: tiescbsp.h:539
Struct for MDIO initialization parameters.
Definition: tiescbsp.h:534
void bsp_set_digio_out(PRUICSS_Handle pruIcssHandle, uint8_t num)
Set selected digital output pin.
uint8_t bsp_get_pdi_access_perm(uint16_t address, uint8_t access)
Checks if the PDI register [byte] has the requested access permission and returns the result.
void bsp_global_mutex_unlock(void)
Critical section leave API using semaphore/mutex/interrupt enable primitives from RTOS....
uint16_t param2low
Definition: tiescbsp.h:501
int32_t interrupt_offset
Definition: tiescbsp.h:436
void bsp_exit(PRUICSS_Handle pruIcssHandle)
Cleanup of EtherCAT FWHAL It does following things: .
Struct for host to PRU-ICSS command interface Starts at PRU0 DMEM.
Definition: tiescbsp.h:492
uint32_t link0_polarity
Definition: tiescbsp.h:456
int32_t bsp_init(bsp_params *init_params)
Initialize the EtherCAT FWHAL It does following things: .
uint32_t bsp_read_dword(PRUICSS_Handle pruIcssHandle, uint16_t address)
Read a 32-bit value at 'Address' from ESC memory: SM mailbox (single buffer) mapped or register area.
void bsp_start_esc_isr(PRUICSS_Handle pruIcssHandle)
Register IRQ handlers for various PRU-ICSS interrupts from firmware to host to clear corresponding ev...
uint32_t bsp_get_timer_register(void)
Returns the time difference from last call of bsp_clear_timer_register to this bsp_get_timer_register...
uint32_t bsp_get_eeprom_updated_time(void)
Get EEPROM Updated time.
PRUICSS_Handle pruicss_handle
Definition: tiescbsp.h:434
void bsp_pruss_cmd_intfc_write_word(uint16_t val, volatile uint16_t *ptr)
Read a 16-bit value from PRU-ICSS IEP command interface.
uint16_t param1low
Definition: tiescbsp.h:500
uint8_t link0pol
Definition: tiescbsp.h:538
uint32_t(* bsp_hwspinlock_lock_t)(int num)
Definition: tiescbsp.h:419
void bsp_get_local_sys_time(uint32_t *systime_low, uint32_t *systime_high)
Return EtherCAT time base for application use.
void bsp_write_dword(PRUICSS_Handle pruIcssHandle, uint32_t val, uint16_t address)
Write a 32-bit value at 'address' in ESC memory.
uint16_t bsp_pruss_cmd_intfc_read_word(volatile uint16_t *ptr)
Read a 16-bit value from PRU-ICSS IEP command interface.
uint16_t reserved
Definition: tisci_boardcfg_rm.h:2
uint32_t bsp_pruss_iepreg_read(PRUICSS_Handle pruIcssHandle, uint32_t regoffset)
Read a 32-bit value from PRU-ICSS IEP register at 'regoffset'.
void bsp_eeprom_emulation_init(void)
Initialize the EEPROM cache in volatile RAM. If the non-volatile storage has valid data(read is perfo...
uint8_t bsp_pdi_access_perm_array(uint16_t address, uint8_t access, uint16_t size)
Checks if all PDI registers starting from 'address' has the requested access permission and returns t...
uint16_t addr
Definition: tiescbsp.h:484
void bsp_set_pdi_perm_read_write(uint16_t *perm_array, uint16_t address)
Set the PDI register [byte] access permission to read and write.
char mode[32]
Definition: tisci_pm_core.h:1
uint32_t phy0_address
Definition: tiescbsp.h:460
bsp_eeprom_write_t eeprom_write
Definition: tiescbsp.h:446
void bsp_clear_timer_register(void)
Update the time when bsp_clear_timer_register last invoked. This is a wrapper API used by SSC.
void Sync1Isr(void *args)
SYNC1 IRQ Handler.
void bsp_pdi_mbx_read_start(PRUICSS_Handle pruIcssHandle)
Indicates to the firmware that PDI side read from write mailbox has started.
uint16_t clkdiv
Definition: tiescbsp.h:535
uint32_t bsp_get_pdi_write_access_fail_cnt()
Returns the count of PDI write access failures.
int8_t(* bsp_get_phy_address_t)(uint8_t instance, uint8_t portNumber)
Definition: tiescbsp.h:422
void bsp_pdi_mbx_read_complete(PRUICSS_Handle pruIcssHandle)
Indicates to the firmware that PDI side read from write mailbox has completed.
void Sync0Isr(void *args)
SYNC0 IRQ handler.
int16_t bsp_pruss_mdio_init(PRUICSS_Handle pruIcssHandle, t_mdio_params *pmdio_params)
Initializes PRU-ICSS MDIO for EtherCAT firmware to communicate with PHYs. Must be called after poweri...
void bsp_pdi_mbx_write_complete(PRUICSS_Handle pruIcssHandle)
Indicates to the firmware that PDI side write to read mailbox has completed.
void bsp_clear_digio_out(PRUICSS_Handle pruIcssHandle, uint8_t num)
Clear selected digital output pin.
t_sm_properties * bsp_get_sm_properties(uint8_t sm)
Get the pointer to requested SM properties. It is used for Buffer/Mailbox read/write detection from H...
bsp_ethercat_stack_isr_function sync1_isr
Definition: tiescbsp.h:473
uint8_t bsp_get_eeprom_update_status(void)
Read the EEPROM update status from FWHAL. Typically called from low priority task periodically check ...
uint16_t cmdlow
Definition: tiescbsp.h:498
uint8_t enhancedlink_enable
Definition: tiescbsp.h:453
int16_t bsp_get_sm_index(uint16_t address, uint16_t len)
void(* bsp_ethercat_stack_isr_function)(void)
Definition: tiescbsp.h:423
uint8_t bsp_read_byte_isr(PRUICSS_Handle pruIcssHandle, uint16_t address)
Read a byte value at 'Address' from ESC process data memory: SM buffer (3-buffer) mapped area.
void bsp_set_digio_sw_dataout_enable(PRUICSS_Handle pruIcssHandle)
Configure digio for sw controlled dataout mode.
void EcatIsr(void *args)
ECAT IRQ Handler.
Struct for FWHAL initialization Parameters.
Definition: tiescbsp.h:433
uint8_t * bsp_get_eeprom_cache_base(void)
Return pointer to volatile EEPROM cache in FWHAL for processing to access the EEPROM.
void bsp_pruss_mdioreg_write(PRUICSS_Handle pruIcssHandle, uint32_t val, uint32_t regoffset)
Write a 32-bit value from PRU-ICSS MDIO register at 'regoffset'.
uint32_t link1_polarity
Definition: tiescbsp.h:458
uint8_t bsp_pdi_sm_config_ongoing(PRUICSS_Handle pruIcssHandle)
Checks whether firmware has finished updating internal state for SM configuration change initiated by...
bsp_ethercat_stack_isr_function sync0_isr
Definition: tiescbsp.h:471
bsp_eeprom_read_t eeprom_read
Definition: tiescbsp.h:444
uint8_t sm_config_ongoing
Definition: tiescbsp.h:496
uint32_t bsp_pruss_mdio_phy_link_state(PRUICSS_Handle pruIcssHandle, uint8_t phyaddr)
Get the link status for selected PHY, this API considers MII_link signal polarity differences and rec...
struct PRUICSS_Config_s * PRUICSS_Handle
A handle that is returned from a PRUICSS_open() call. This handle is required for calling other APIs.
Definition: pruicss/v0/pruicss.h:234
uint16_t physical_start_addr
Definition: tiescbsp.h:526
const unsigned char * default_tiesc_eeprom
Definition: tiescbsp.h:464
void bsp_get_latch0_negedge_time(PRUICSS_Handle pruIcssHandle, uint32_t *systime_low, uint32_t *systime_high)
Return latch0 negedge timestamp for application use(nanosec resolution)
void bsp_hwspinlock_init(void)
Initialize SOC spinlock, enable clocks and init spinlock instance 0 through 7 to unlocked state.