5. Installing the Compiler¶
Note
The typical use model for the compiler is to invoke it from within EdgeAI Studio or Tiny ML ModelMaker.
5.1. Installing¶
TI Neural Network Compiler for MCUs is distributed as a prebuilt Python package in wheel format. It can be installed using a standard Python wheel installation mechanism. For example:
pip3 install ./ti_mcu_nnc-1.2.0-cp310-cp310-linux_x86_64.whl
5.2. Verifying install¶
After installation, verify that the compiler is available as follows:
which tvmc python3 -c "import tvm; print(tvm.__file__)" ls `python3 -c "import tvm; print(tvm.__path__[0])"`/ti_docs/index.html