![]() |
0.01.00
|
This is the complete list of members for ot::MessagePool, including all inherited members.
| Free(Message *aMessage) | ot::MessagePool | |
| GetAllMessagesHead(void) const | ot::MessagePool | |
| GetAllMessagesTail(void) const | ot::MessagePool | inline |
| GetFreeBufferCount(void) const | ot::MessagePool | inline |
| GetInstance(void) const | ot::InstanceLocator | inline |
| GetIp6(void) const | ot::InstanceLocator | |
| GetNetif(void) const | ot::InstanceLocator | |
| InstanceLocator(otInstance &aInstance) | ot::InstanceLocator | inlineprotected |
| Message (defined in ot::MessagePool) | ot::MessagePool | friend |
| MessagePool(otInstance &aInstance) | ot::MessagePool | |
| MessageQueue (defined in ot::MessagePool) | ot::MessagePool | friend |
| New(uint8_t aType, uint16_t aReserveHeader) | ot::MessagePool | |
| PriorityQueue (defined in ot::MessagePool) | ot::MessagePool | friend |