![]() |
0.01.00
|
This is the complete list of members for ot::AnnounceBeginServer, including all inherited members.
| AnnounceBeginServer(otInstance &aInstance) | ot::AnnounceBeginServer | |
| GetInstance(void) const | ot::InstanceLocator | inline |
| GetIp6(void) const | ot::InstanceLocator | |
| GetNetif(void) const | ot::InstanceLocator | |
| InstanceLocator(otInstance &aInstance) | ot::InstanceLocator | inlineprotected |
| SendAnnounce(uint32_t aChannelMask) | ot::AnnounceBeginServer | |
| SendAnnounce(uint32_t aChannelMask, uint8_t aCount, uint16_t aPeriod) | ot::AnnounceBeginServer |