![]() |
0.01.00
|
This is the complete list of members for ot::Timer, including all inherited members.
| Context(void *aContext) | ot::Context | inlineprotected |
| DoesFireBefore(const Timer &aTimer, uint32_t aNow) | ot::Timer | protected |
| Fired(void) (defined in ot::Timer) | ot::Timer | inlineprotected |
| GetFireTime(void) const | ot::Timer | inline |
| GetInstance(void) const | ot::InstanceLocator | inline |
| GetIp6(void) const | ot::InstanceLocator | |
| GetNetif(void) const | ot::InstanceLocator | |
| Handler typedef | ot::Timer | |
| InstanceLocator(otInstance &aInstance) | ot::InstanceLocator | inlineprotected |
| IsRunning(void) const | ot::Timer | inline |
| kMaxDt enum value (defined in ot::Timer) | ot::Timer | |
| mFireTime (defined in ot::Timer) | ot::Timer | protected |
| mHandler (defined in ot::Timer) | ot::Timer | protected |
| mNext (defined in ot::Timer) | ot::Timer | protected |
| Timer(otInstance &aInstance, Handler aHandler, void *aContext) | ot::Timer | inline |
| TimerScheduler (defined in ot::Timer) | ot::Timer | friend |