0.01.00
ot::KeyManager Member List

This is the complete list of members for ot::KeyManager, including all inherited members.

GetCurrentKeySequence(void) constot::KeyManagerinline
GetCurrentMacKey(void) constot::KeyManagerinline
GetCurrentMleKey(void) constot::KeyManagerinline
GetInstance(void) constot::InstanceLocatorinline
GetIp6(void) constot::InstanceLocator
GetKek(void) constot::KeyManagerinline
GetKekFrameCounter(void) constot::KeyManagerinline
GetKeyRotation(void) constot::KeyManagerinline
GetKeySwitchGuardTime(void) constot::KeyManagerinline
GetMacFrameCounter(void) constot::KeyManagerinline
GetMasterKey(void) constot::KeyManager
GetMleFrameCounter(void) constot::KeyManagerinline
GetNetif(void) constot::InstanceLocator
GetPSKc(void) constot::KeyManager
GetSecurityPolicyFlags(void) constot::KeyManagerinline
GetTemporaryMacKey(uint32_t aKeySequence)ot::KeyManager
GetTemporaryMleKey(uint32_t aKeySequence)ot::KeyManager
IncrementKekFrameCounter(void)ot::KeyManagerinline
IncrementMacFrameCounter(void)ot::KeyManager
IncrementMleFrameCounter(void)ot::KeyManager
InstanceLocator(otInstance &aInstance)ot::InstanceLocatorinlineprotected
KeyManager(otInstance &aInstance)ot::KeyManagerexplicit
kMaxKeyLength enum value (defined in ot::KeyManager)ot::KeyManager
SetCurrentKeySequence(uint32_t aKeySequence)ot::KeyManager
SetKek(const uint8_t *aKek)ot::KeyManager
SetKeyRotation(uint32_t aKeyRotation)ot::KeyManager
SetKeySwitchGuardTime(uint32_t aKeySwitchGuardTime)ot::KeyManagerinline
SetMacFrameCounter(uint32_t aMacFrameCounter)ot::KeyManagerinline
SetMasterKey(const otMasterKey &aKey)ot::KeyManager
SetMleFrameCounter(uint32_t aMleFrameCounter)ot::KeyManagerinline
SetPSKc(const uint8_t *aPSKc)ot::KeyManager
SetSecurityPolicyFlags(uint8_t aSecurityPolicyFlags)ot::KeyManagerinline
SetStoredMacFrameCounter(uint32_t aStoredMacFrameCounter)ot::KeyManagerinline
SetStoredMleFrameCounter(uint32_t aStoredMleFrameCounter)ot::KeyManagerinline
Start(void)ot::KeyManager
Stop(void)ot::KeyManager