0.01.00
crc16.hpp
Go to the documentation of this file.
1 /*
2  * Copyright (c) 2016, The OpenThread Authors.
3  * All rights reserved.
4  *
5  * Redistribution and use in source and binary forms, with or without
6  * modification, are permitted provided that the following conditions are met:
7  * 1. Redistributions of source code must retain the above copyright
8  * notice, this list of conditions and the following disclaimer.
9  * 2. Redistributions in binary form must reproduce the above copyright
10  * notice, this list of conditions and the following disclaimer in the
11  * documentation and/or other materials provided with the distribution.
12  * 3. Neither the name of the copyright holder nor the
13  * names of its contributors may be used to endorse or promote products
14  * derived from this software without specific prior written permission.
15  *
16  * THIS SOFTWARE IS PROVIDED BY THE COPYRIGHT HOLDERS AND CONTRIBUTORS "AS IS"
17  * AND ANY EXPRESS OR IMPLIED WARRANTIES, INCLUDING, BUT NOT LIMITED TO, THE
18  * IMPLIED WARRANTIES OF MERCHANTABILITY AND FITNESS FOR A PARTICULAR PURPOSE
19  * ARE DISCLAIMED. IN NO EVENT SHALL THE COPYRIGHT HOLDER OR CONTRIBUTORS BE
20  * LIABLE FOR ANY DIRECT, INDIRECT, INCIDENTAL, SPECIAL, EXEMPLARY, OR
21  * CONSEQUENTIAL DAMAGES (INCLUDING, BUT NOT LIMITED TO, PROCUREMENT OF
22  * SUBSTITUTE GOODS OR SERVICES; LOSS OF USE, DATA, OR PROFITS; OR BUSINESS
23  * INTERRUPTION) HOWEVER CAUSED AND ON ANY THEORY OF LIABILITY, WHETHER IN
24  * CONTRACT, STRICT LIABILITY, OR TORT (INCLUDING NEGLIGENCE OR OTHERWISE)
25  * ARISING IN ANY WAY OUT OF THE USE OF THIS SOFTWARE, EVEN IF ADVISED OF THE
26  * POSSIBILITY OF SUCH DAMAGE.
27  */
28 
34 #ifndef CRC16_HPP_
35 #define CRC16_HPP_
36 
37 #include "openthread-core-config.h"
38 
39 #include "utils/wrap_stdint.h"
40 
41 namespace ot {
42 
47 class Crc16
48 {
49 public:
51  {
52  kCcitt = 0x1021,
53  kAnsi = 0x8005,
54  };
55 
62  Crc16(Polynomial aPolynomial);
63 
68  void Init(void) { mCrc = 0; }
69 
70  /*c*
71  * This method feeds a byte value into the CRC16 computation.
72  *
73  * @param[in] aByte The byte value.
74  *
75  */
76  void Update(uint8_t aByte);
77 
84  uint16_t Get(void) const { return mCrc; }
85 
86 private:
87  uint16_t mPolynomial;
88  uint16_t mCrc;
89 };
90 
91 } // namespace ot
92 
93 #endif // CRC16_HPP_
uint16_t Get(void) const
This method gets the current CRC16 value.
Definition: crc16.hpp:84
Definition: cli.cpp:90
CRC16_CCITT.
Definition: crc16.hpp:52
void Init(void)
This method initializes the CRC16 computation.
Definition: crc16.hpp:68
Polynomial
Definition: crc16.hpp:50
This class implements CRC16 computations.
Definition: crc16.hpp:47
This file includes compile-time configuration constants for OpenThread.
CRC16-ANSI.
Definition: crc16.hpp:53
Crc16(Polynomial aPolynomial)
This constructor initializes the object.
Definition: crc16.cpp:38