0.01.00
ot::Router Member List

This is the complete list of members for ot::Router, including all inherited members.

ClearExtAddress(void)ot::Neighborinline
GenerateChallenge(void)ot::Neighbor
GetChallenge(void) constot::Neighborinline
GetChallengeSize(void) constot::Neighborinline
GetCost(void) constot::Routerinline
GetDeviceMode(void) constot::Neighborinline
GetExtAddress(void)ot::Neighborinline
GetExtAddress(void) constot::Neighborinline
GetKeySequence(void) constot::Neighborinline
GetLastHeard(void) constot::Neighborinline
GetLinkFailures(void) constot::Neighborinline
GetLinkFrameCounter(void) constot::Neighborinline
GetLinkInfo(void)ot::Neighborinline
GetLinkQualityOut(void) constot::Routerinline
GetMleFrameCounter(void) constot::Neighborinline
GetNextHop(void) constot::Routerinline
GetRloc16(void) constot::Neighborinline
GetState(void) constot::Neighborinline
IncrementLinkFailures(void)ot::Neighborinline
IsAllocated(void) constot::Routerinline
IsDataRequestPending(void) constot::Neighborinline
IsFullNetworkData(void) constot::Neighborinline
IsFullThreadDevice(void) constot::Neighborinline
IsReclaimDelay(void) constot::Routerinline
IsRxOnWhenIdle(void) constot::Neighborinline
IsSecureDataRequest(void) constot::Neighborinline
IsStateRestoring(void) constot::Neighborinline
IsStateValidOrRestoring(void) constot::Neighborinline
kStateChildIdRequest enum valueot::Neighbor
kStateChildUpdateRequest enum valueot::Neighbor
kStateInvalid enum valueot::Neighbor
kStateLinkRequest enum valueot::Neighbor
kStateParentRequest enum valueot::Neighbor
kStateRestored enum valueot::Neighbor
kStateValid enum valueot::Neighbor
mChallengeot::Neighbor
mChallengeLengthot::Neighbor
mLinkFrameCounterot::Neighbor
mMleFrameCounterot::Neighbor
mPending (defined in ot::Neighbor)ot::Neighbor
mRloc16ot::Neighbor
mValid (defined in ot::Neighbor)ot::Neighbor
ResetLinkFailures(void)ot::Neighborinline
SetAllocated(bool aAllocated)ot::Routerinline
SetCost(uint8_t aCost)ot::Routerinline
SetDataRequestPending(bool aPending)ot::Neighborinline
SetDeviceMode(uint8_t aMode)ot::Neighborinline
SetExtAddress(const Mac::ExtAddress &aAddress)ot::Neighborinline
SetKeySequence(uint32_t aKeySequence)ot::Neighborinline
SetLastHeard(uint32_t aLastHeard)ot::Neighborinline
SetLinkFrameCounter(uint32_t aFrameCounter)ot::Neighborinline
SetLinkQualityOut(uint8_t aLinkQuality)ot::Routerinline
SetMleFrameCounter(uint32_t aFrameCounter)ot::Neighborinline
SetNextHop(uint8_t aRouterId)ot::Routerinline
SetReclaimDelay(bool aReclaimDelay)ot::Routerinline
SetRloc16(uint16_t aRloc16)ot::Neighborinline
SetState(State aState)ot::Neighborinline
State enum nameot::Neighbor