|  | 
| Clock_Handle | Util_constructClock (Clock_Struct *pClock, Clock_FuncPtr clockCB, uint32_t clockDuration, uint32_t clockPeriod, uint8_t startFlag, UArg arg) | 
|  | Initialize a TIRTOS Clock instance.  More... 
 | 
|  | 
| Queue_Handle | Util_constructQueue (Queue_Struct *pQueue) | 
|  | Initialize an RTOS queue to hold messages from profile to be processed.  More... 
 | 
|  | 
| char * | Util_convertBdAddr2Str (uint8_t *pAddr) | 
|  | Convert Bluetooth address to string. Only needed when LCD display is used.  More... 
 | 
|  | 
| uint8_t * | Util_dequeueMsg (Queue_Handle msgQueue) | 
|  | Dequeues the message from the RTOS queue.  More... 
 | 
|  | 
| uint8_t | Util_enqueueMsg (Queue_Handle msgQueue, Event_Handle event, uint8_t *pMsg) | 
|  | Creates a queue node and puts the node in RTOS queue.  More... 
 | 
|  | 
| bool | Util_isActive (Clock_Struct *pClock) | 
|  | Determine if a clock is currently active.  More... 
 | 
|  | 
| uint8_t | Util_isBufSet (uint8_t *pBuf, uint8_t pattern, uint16_t len) | 
|  | Check if contents of buffer matches byte pattern.  More... 
 | 
|  | 
| void | Util_rescheduleClock (Clock_Struct *pClock, uint32_t clockPeriod) | 
|  | Reschedule a clock by changing the timeout and period values.  More... 
 | 
|  | 
| void | Util_restartClock (Clock_Struct *pClock, uint32_t clockTimeout) | 
|  | Restart a clock by changing the timeout.  More... 
 | 
|  | 
| void | Util_startClock (Clock_Struct *pClock) | 
|  | Start a clock.  More... 
 | 
|  | 
| void | Util_stopClock (Clock_Struct *pClock) | 
|  | Stop a clock.  More... 
 | 
|  |