x_x___params.html" title="ECCROMCC26XX Parameters. ">ECCROMCC26XX_Params struct to its defaults. params should not be modified until after this function is called. Default parameters use the NIST P-256 curve, timeout is set to wait indefinitely, malloc and free are NULL and status is set to ECCROMCC26XX_STATUS_SUCCESS. A client may call this function with the same params instance any number of times.

Precondition
Calling context: Hwi, Swi and Task.
Parameters
paramsParameter structure to initialize.
Copyright 2018, Texas Instruments Incorporated