39 #include <ti/sysbios/knl/Queue.h> 54 #define UB_PARAM_COMMON_START 0 67 #define UB_PARAM_RFPRIORITY (UB_PARAM_COMMON_START+0) 76 #define UB_PARAM_TXPOWER (UB_PARAM_COMMON_START+1) 79 #define UB_PARAM_COMMON_END UB_PARAM_TXPOWER 80 #if defined(FEATURE_ADVERTISER) 81 #define UB_PARAM_ADV_CMN_START (UB_PARAM_COMMON_END+1) 91 #define UB_PARAM_ADVINTERVAL (UB_PARAM_ADV_CMN_START+0) 99 #define UB_PARAM_ADVCHANMAP (UB_PARAM_ADV_CMN_START+1) 107 #define UB_PARAM_ADVTYPE (UB_PARAM_ADV_CMN_START+2) 119 #define UB_PARAM_TIMETOADV (UB_PARAM_ADV_CMN_START+3) 127 #define UB_PARAM_ADVDATA (UB_PARAM_ADV_CMN_START+4) 130 #define UB_PARAM_ADV_CMN_END UB_PARAM_ADVDATA 131 #if defined(FEATURE_SCAN_RESPONSE) 132 #define UB_PARAM_ADV_SR_START (UB_PARAM_ADV_CMN_END+1) 142 #define UB_PARAM_SCANRSPDATA (UB_PARAM_ADV_SR_START+0) 152 #define UB_PARAM_ADVFLTPOLICY (UB_PARAM_ADV_SR_START+1) 155 #define UB_PARAM_ADV_SR_END UB_PARAM_ADVFLTPOLICY 157 #define UB_PARAM_ADV_SR_END UB_PARAM_ADV_CMN_END 160 #define UB_PARAM_ADV_SR_END UB_PARAM_COMMON_END 162 #if defined(FEATURE_SCANNER) 163 #define UB_PARAM_SCAN_START (UB_PARAM_ADV_SR_END+1) 164 #define UB_PARAM_SCANINTERVAL (UB_PARAM_SCAN_START+0) 165 #define UB_PARAM_SCANWINDOW (UB_PARAM_SCAN_START+1) 166 #define UB_PARAM_SCANCHANMAP (UB_PARAM_SCAN_START+2) 167 #define UB_PARAM_SCANTYPE (UB_PARAM_SCAN_START+3) 168 #define UB_PARAM_FLTDUPLICATE (UB_PARAM_SCAN_START+4) 169 #define UB_PARAM_SCANFLTPOLICY (UB_PARAM_SCAN_START+5) 170 #define UB_PARAM_SCAN_END UB_PARAM_SCANFLTPOLICY 172 #define UB_PARAM_SCAN_END UB_PARAM_ADV_SR_END 174 #define UB_NUM_PARAM (UB_PARAM_SCAN_END+1) 181 #define RF_PRI_NORMAL ((uint8) RF_PriorityNormal) 182 #define RF_PRI_HIGH ((uint8) RF_PriorityHigh) 183 #define RF_PRI_HIGHEST ((uint8) RF_PriorityHighest) 189 #define RF_TIME_RELAXED 0 190 #define RF_TIME_CRITICAL 1 194 #define UB_TX_POWER_INVALID 0xFFFF 199 #define UB_ADDRTYPE_PUBLIC 0 200 #define UB_ADDRTYPE_STATIC 1 201 #define UB_ADDRTYPE_NONRESOLVABLE 2 202 #define UB_ADDRTYPE_RESOLVABLE 3 203 #define UB_ADDRTYPE_BD 4 209 #define UB_ADVTYPE_ADV_NC 5 210 #define UB_ADVTYPE_ADV_SCAN 6 217 #define UB_ADV_CHAN_37 0x01 218 #define UB_ADV_CHAN_38 0x02 219 #define UB_ADV_CHAN_39 0x04 220 #define UB_ADV_CHAN_ALL (UB_ADV_CHAN_37 | UB_ADV_CHAN_38 | UB_ADV_CHAN_39) 224 #define UB_MIN_ADV_INTERVAL 160 225 #define UB_MAX_ADV_INTERVAL 16384 226 #define UB_MIN_CHANNEL_MAP UB_ADV_CHAN_37 227 #define UB_MAX_CHANNEL_MAP UB_ADV_CHAN_ALL 228 #define UB_MIN_TX_POWER TX_POWER_MINUS_21_DBM 229 #define UB_MAX_TX_POWER TX_POWER_5_DBM 233 #define UB_PARAM_DFLT_RFPRIORITY RF_PRI_NORMAL 234 #define UB_PARAM_DFLT_RFTIMECRIT RF_TIME_RELAXED 235 #define UB_PARAM_DFLT_TXPOWER TX_POWER_0_DBM 236 #define UB_PARAM_DFLT_ADVINTERVAL 1600 237 #define UB_PARAM_DFLT_ADVCHANMAP UB_ADV_CHAN_ALL 238 #define UB_PARAM_DFLT_ADVTYPE UB_ADVTYPE_ADV_NC 239 #define UB_PARAM_DFLT_TIMETOADV 0 240 #define UB_PARAM_DFLT_ADVDATA {0} 241 #define UB_PARAM_DFLT_SCANRSPDATA {0} 242 #define UB_PARAM_DFLT_ADVFLTPOLICY 0 248 #define UB_EVTDST_LL 0 249 #define UB_EVTDST_GAP 1 250 #define UB_NUM_EVTDST 2 258 #define MS_TO_RAT 4000 260 #define BLE_TO_RAT 2500 262 #define SYSTICK_TO_RAT (Clock_tickPeriod * US_TO_RAT) 264 #define MS_TO_SYSTICK (1000 / Clock_tickPeriod) 266 #define BYTE_TO_RAT (8 * US_TO_RAT) 269 #define UB_MAX_ADVDATA_LEN B_MAX_ADV_LEN 290 PACKED_TYPEDEF_STRUCT {
299 PACKED_TYPEDEF_STRUCT {
328 PACKED_TYPEDEF_STRUCT {
331 #if defined(FEATURE_ADVERTISER) 337 #if defined(FEATURE_SCAN_RESPONSE) 342 #if defined(FEATURE_SCANNER) 357 PACKED_TYPEDEF_STRUCT {
void ub_resetAddr(void)
Make BD Addr revert to Random Static Address if exists or Public Address otherwise.
void(* ubPostEvtProxyCB_t)(void)
Type of the callback to have ub_processMsg called in the application task context.
Definition: uble.h:317
bStatus_t ub_checkAddr(ubAddrType_t addrType, uint8 *pAddr)
Check if the given address is valid.
bStatus_t ub_getParameter(uint8 param, void *pValue)
Get a Micro BLE Stack parameter.
bStatus_t ub_setParameter(uint8 param, uint8 len, void *pValue)
Set a Micro BLE Stack parameter.
#define UB_MAX_ADVDATA_LEN
Max Advertising Data Length.
Definition: uble.h:269
uint8 ubEvt_t
Micro BLE Stack Event.
Definition: uble.h:288
uint8 ubAddrType_t
Address Type.
Definition: uble.h:282
uint8 ubMsg_t
Type of Micro BLE Stack message.
Definition: uble.h:297
bStatus_t ub_stackInit(ubAddrType_t addrType, uint8 *pStaticAddr, ubPostEvtProxyCB_t pfnPostEvtProxyCB, uint8 timeCritical)
Initialize Micro BLE Stack.
void ub_processMsg(void)
Let the Micro Stack process the queued messages.
Status_t bStatus_t
BLE Generic Status return.
Definition: bcomdef.h:225
bStatus_t ub_getAddr(ubAddrType_t addrType, uint8 *pAddr)
Retrieve the address corresponding to the given address type.
uint8 ubEvtDst_t
Recipient of Micro BLE Stack Event.
Definition: uble.h:285
This file contains configurable variables for the Micro BLE Stack radio.
void(* ubProcessMsg_t)(ubEvtMsg_t *pEvtMsg)
Function to process event messages destined to the calle module.
Definition: uble.h:322