Simple Peripheral OAD Off-chip
Table of Contents
Introduction
The simple_peripheral_oad_offchip project demonstrates off-chip OAD functionality with the simple_peripheral application. The application behavior is the same as the stock simple_peripheral project, with the exception that OAD is added.
Note: The bim_oad_offchip
project must also be flashed to the device when using off-chip OAD or the device will not function correctly
This project uses stack and app configurations that are summarized in the table below:
App Build Configuration | Compatible Stack Configuration | Description |
---|---|---|
FlashROM_OAD_Offchip | FlashROM | OAD off chip application FlashROM configuration |
FlashROM configurations use the split image configuration, which is explained here.
This document seeks to extend the simple_peripheral project documentation that is already in place, and explain how simple_peripheral can be used to demonstrate off-chip OAD. For an advanced discussion of OAD, and an in-depth explanation of this project, please see:
** Off-chip OAD Software Developer’s Guide Section**
Hardware Prerequisites
The default Simple Peripheral OAD-offchip configuration uses the LAUNCHXL-CC2640R2. This hardware configuration is shown in the below image:
For custom hardware, see the Running the SDK on Custom Boards section of the TI Bluetooth low energy Software Developer’s Guide.
Software Prerequisites
For information on what versions of Code Composer Studio and IAR Embedded Workbench to use, see the Release Notes located in the docs/blestack folder. For information on how to import this project into your IDE workspace and build/run, please refer to The CC2640R2F Platform section in the Bluetooth low energy Software Developer’s Guide.
Service/Profile Table
This project contains the simple service, which has 5 characteristics.
Note that BLE Scanner may report 128 bit UUIDs, but the project is generating 16 bit UUIDs.
Characterisitic | UUID | Format | Properties | Profile Source |
---|---|---|---|---|
1 | FFF1 | 1 Byte Integer | Read/Write | simple_gatt_profile.c |
2 | FFF2 | 1 Byte Integer | Read | simple_gatt_profile.c |
3 | FFF3 | 1 Byte Integer | Write | simple_gatt_profile.c |
4 | FFF4 | 1 Byte Integer | Notify | simple_gatt_profile.c |
5 | FFF5 | 5 Byte Integer | Read | simple_gatt_profile.c |
Additionally, this project contains the OAD profile, which has 5 characteristics.
See ** OAD Service Description in Software Developer’s Guide** for more information on the OAD service
Usage
This application uses the UART peripheral to provide an interface for the application. The UART is only used for display messages.
This document will use PuTTY to serve as the display for the output of the CC2640R2 LaunchPad, and it will use BLE Scanner as the phone app that will act as the central device that will connect to the Simple Peripheral device. Note that any other serial terminal and smart phone BLE application can be used. The following default parameters are used for the UART peripheral for display:
UART Param | Default Values |
---|---|
Baud Rate | 115200 |
Data length | 8 bits |
Parity | None |
Stop bits | 1 bit |
Flow Control | None |
For further guidance refer to ** Off-chip OAD Software Developer’s Guide Section**