Go to the source code of this file.
|
Clock_Handle | Util_constructClock (Clock_Struct *pClock, Clock_FuncPtr clockCB, uint32_t clockDuration, uint32_t clockPeriod, uint8_t startFlag, UArg arg) |
| Initialize a TIRTOS Clock instance. More...
|
|
Queue_Handle | Util_constructQueue (Queue_Struct *pQueue) |
| Initialize an RTOS queue to hold messages from profile to be processed. More...
|
|
uint8_t * | Util_dequeueMsg (Queue_Handle msgQueue) |
| Dequeue the message from the RTOS queue. More...
|
|
uint8_t | Util_enqueueMsg (Queue_Handle msgQueue, Event_Handle event, uint8_t *pMsg) |
| Creates a queue node and puts the node in RTOS queue. More...
|
|
bool | Util_isActive (Clock_Struct *pClock) |
| Determine if a clock is currently active. More...
|
|
void | Util_rescheduleClock (Clock_Struct *pClock, uint32_t clockPeriod) |
| Reschedule a clock by changing the timeout and period values. More...
|
|
void | Util_restartClock (Clock_Struct *pClock, uint32_t clockTimeout) |
| Restart a clock by changing the timeout. More...
|
|
void | Util_startClock (Clock_Struct *pClock) |
| Start a clock. More...
|
|
void | Util_stopClock (Clock_Struct *pClock) |
| Stop a clock. More...
|
|