Go to the documentation of this file. 32 #include "hal_types.h" 77 #define INVALIDPARAMETER 0x02 78 #define INVALID_TASK 0x03 79 #define MSG_BUFFER_NOT_AVAIL 0x04 80 #define INVALID_MSG_POINTER 0x05 81 #define INVALID_EVENT_ID 0x06 82 #define INVALID_INTERRUPT_ID 0x07 83 #define NO_TIMER_AVAIL 0x08 84 #define NV_ITEM_UNINIT 0x09 85 #define NV_OPER_FAILED 0x0A 86 #define INVALID_MEM_SIZE 0x0B 87 #define NV_BAD_ITEM_LEN 0x0C 96 typedef uint8 Status_t;
100 typedef uint32 uint24;
108 #define SYS_EVENT_MSG 0x8000 114 #define KEY_CHANGE 0xC0
Copyright 2017, Texas Instruments Incorporated