Instance: I2S0
Component: I2S
Base address: 0x40021000
I2S Audio DMA module supporting formats I2S, LJF, RJF and DSP
|
Register Name |
Type |
Register Width (Bits) |
Register Reset |
Address Offset |
Physical Address |
|
RW |
32 |
0x0000 0000 |
0x0000 0000 |
0x4002 1000 |
|
|
RW |
32 |
0x0000 0000 |
0x0000 0004 |
0x4002 1004 |
|
|
RW |
32 |
0x0000 0000 |
0x0000 0008 |
0x4002 1008 |
|
|
RW |
32 |
0x0000 0170 |
0x0000 000C |
0x4002 100C |
|
|
RW |
32 |
0x0000 0003 |
0x0000 0010 |
0x4002 1010 |
|
|
RW |
32 |
0x0000 0003 |
0x0000 0014 |
0x4002 1014 |
|
|
RW |
32 |
0x0000 0000 |
0x0000 001C |
0x4002 101C |
|
|
RW |
32 |
0x0000 0000 |
0x0000 0020 |
0x4002 1020 |
|
|
RW |
32 |
0x0000 0000 |
0x0000 0024 |
0x4002 1024 |
|
|
RW |
32 |
0x0000 0000 |
0x0000 0028 |
0x4002 1028 |
|
|
RW |
32 |
0x0000 0000 |
0x0000 002C |
0x4002 102C |
|
|
RW |
32 |
0x0000 0000 |
0x0000 0034 |
0x4002 1034 |
|
|
RO |
32 |
0x0000 0000 |
0x0000 0038 |
0x4002 1038 |
|
|
RO |
32 |
0x0000 0000 |
0x0000 003C |
0x4002 103C |
|
|
RO |
32 |
0x0000 0000 |
0x0000 0040 |
0x4002 1040 |
|
|
RW |
32 |
0x0000 0000 |
0x0000 0044 |
0x4002 1044 |
|
|
RW |
32 |
0x0000 0000 |
0x0000 0048 |
0x4002 1048 |
|
|
RW |
32 |
0x0000 0000 |
0x0000 004C |
0x4002 104C |
|
|
RW |
32 |
0x0000 0000 |
0x0000 0050 |
0x4002 1050 |
|
|
RW |
32 |
0x0000 0000 |
0x0000 0054 |
0x4002 1054 |
|
|
RW |
32 |
0x0000 FFFF |
0x0000 0058 |
0x4002 1058 |
|
|
RO |
32 |
0x0000 0000 |
0x0000 005C |
0x4002 105C |
|
|
RO |
32 |
0x0000 0000 |
0x0000 0060 |
0x4002 1060 |
|
|
RO |
32 |
0x0000 0000 |
0x0000 0064 |
0x4002 1064 |
|
|
RO |
32 |
0x0000 0000 |
0x0000 0068 |
0x4002 1068 |
|
|
RW |
32 |
0x0000 0000 |
0x0000 0070 |
0x4002 1070 |
|
|
RO |
32 |
0x0000 0000 |
0x0000 0074 |
0x4002 1074 |
|
|
WO |
32 |
0x0000 0000 |
0x0000 0078 |
0x4002 1078 |
|
|
WO |
32 |
0x0000 0000 |
0x0000 007C |
0x4002 107C |
| Address Offset | 0x0000 0000 | ||
| Physical Address | 0x4002 1000 | Instance | 0x4002 1000 |
| Description | WCLK Source Selection | ||
| Type | RW | ||
| Bits | Field Name | Description | Type | Reset | |||||||||||||||||
| 31:3 | RESERVED3 | Software should not rely on the value of a reserved. Writing any other value than the reset value may result in undefined behavior. | RO | 0b0 0000 0000 0000 0000 0000 0000 0000 | |||||||||||||||||
| 2 | WCLK_INV | Inverts WCLK source (pad or internal) when set. 0: Not inverted 1: Inverted |
RW | 0 | |||||||||||||||||
| 1:0 | WCLK_SRC | Selects WCLK source for AIF (should be the same as the BCLK source). The BCLK source is defined in the PRCM:I2SBCLKSEL.SRC
|
RW | 0b00 | |||||||||||||||||
| Address Offset | 0x0000 0004 | ||
| Physical Address | 0x4002 1004 | Instance | 0x4002 1004 |
| Description | DMA Buffer Size Configuration | ||
| Type | RW | ||
| Bits | Field Name | Description | Type | Reset | ||
| 31:8 | RESERVED8 | Software should not rely on the value of a reserved. Writing any other value than the reset value may result in undefined behavior. | RO | 0x00 0000 | ||
| 7:0 | END_FRAME_IDX | Defines the length of the DMA buffer. Writing a non-zero value to this register field enables and initializes AIF. Note that before doing so, all other configuration must have been done, and AIFINPTRNEXT/AIFOUTPTRNEXT must have been loaded. | RW | 0x00 | ||
| Address Offset | 0x0000 0008 | ||
| Physical Address | 0x4002 1008 | Instance | 0x4002 1008 |
| Description | Pin Direction | ||
| Type | RW | ||
| Bits | Field Name | Description | Type | Reset | ||||||||||||||
| 31:10 | RESERVED10 | Software should not rely on the value of a reserved. Writing any other value than the reset value may result in undefined behavior. | RO | 0b00 0000 0000 0000 0000 0000 | ||||||||||||||
| 9:8 | AD2 | Configures the AD2 audio data pin usage 0x3: Reserved
|
RW | 0b00 | ||||||||||||||
| 7:6 | RESERVED6 | Software should not rely on the value of a reserved. Writing any other value than the reset value may result in undefined behavior. | RO | 0b00 | ||||||||||||||
| 5:4 | AD1 | Configures the AD1 audio data pin usage: 0x3: Reserved
|
RW | 0b00 | ||||||||||||||
| 3:2 | RESERVED2 | Software should not rely on the value of a reserved. Writing any other value than the reset value may result in undefined behavior. | RO | 0b00 | ||||||||||||||
| 1:0 | AD0 | Configures the AD0 audio data pin usage: 0x3: Reserved
|
RW | 0b00 | ||||||||||||||
| Address Offset | 0x0000 000C | ||
| Physical Address | 0x4002 100C | Instance | 0x4002 100C |
| Description | Serial Interface Format Configuration | ||
| Type | RW | ||
| Bits | Field Name | Description | Type | Reset | |||||||||||
| 31:16 | RESERVED16 | Software should not rely on the value of a reserved. Writing any other value than the reset value may result in undefined behavior. | RO | 0x0000 | |||||||||||
| 15:8 | DATA_DELAY | The number of BCLK periods between a WCLK edge and MSB of the first word in a phase: 0x00: LJF format 0x01: I2S and DSP format 0x02: RJF format ... 0xFF: RJF format Note: When 0, MSB of the next word will be output in the idle period between LSB of the previous word and the start of the next word. Otherwise logical 0 will be output until the data delay has expired. |
RW | 0x01 | |||||||||||
| 7 | MEM_LEN_24 | The size of each word stored to or loaded from memory:
|
RW | 0 | |||||||||||
| 6 | SMPL_EDGE | On the serial audio interface, data (and wclk) is sampled and clocked out on opposite edges of BCLK.
|
RW | 1 | |||||||||||
| 5 | DUAL_PHASE | Selects dual- or single-phase format. 0: Single-phase: DSP format 1: Dual-phase: I2S, LJF and RJF formats |
RW | 1 | |||||||||||
| 4:0 | WORD_LEN | Number of bits per word (8-24): In single-phase format, this is the exact number of bits per word. In dual-phase format, this is the maximum number of bits per word. Values below 8 and above 24 give undefined behavior. Data written to memory is always aligned to 16 or 24 bits as defined by MEM_LEN_24. Bit widths that differ from this alignment will either be truncated or zero padded. |
RW | 0b1 0000 | |||||||||||
| Address Offset | 0x0000 0010 | ||
| Physical Address | 0x4002 1010 | Instance | 0x4002 1010 |
| Description | Word Selection Bit Mask for Pin 0 | ||
| Type | RW | ||
| Bits | Field Name | Description | Type | Reset | ||
| 31:8 | RESERVED8 | Software should not rely on the value of a reserved. Writing any other value than the reset value may result in undefined behavior. | RW | 0x00 0000 | ||
| 7:0 | MASK | Bit-mask indicating valid channels in a frame on AD0. In single-phase mode, each bit represents one channel, starting with LSB for the first word in the frame. A frame can contain up to 8 channels. Channels that are not included in the mask will not be sampled and stored in memory, and clocked out as '0'. In dual-phase mode, only the two LSBs are considered. For a stereo configuration, set both bits. For a mono configuration, set bit 0 only. In mono mode, only channel 0 will be sampled and stored to memory, and channel 0 will be repeated when clocked out. In mono mode, only channel 0 will be sampled and stored to memory, and channel 0 will be repeated in the second phase when clocked out. If all bits are zero, no input words will be stored to memory, and the output data lines will be constant '0'. This can be utilized when PWM debug output is desired without any actively used output pins. |
RW | 0x03 | ||
| Address Offset | 0x0000 0014 | ||
| Physical Address | 0x4002 1014 | Instance | 0x4002 1014 |
| Description | Word Selection Bit Mask for Pin 1 | ||
| Type | RW | ||
| Bits | Field Name | Description | Type | Reset | ||
| 31:8 | RESERVED8 | Software should not rely on the value of a reserved. Writing any other value than the reset value may result in undefined behavior. | RO | 0x00 0000 | ||
| 7:0 | MASK | Bit-mask indicating valid channels in a frame on AD1. In single-phase mode, each bit represents one channel, starting with LSB for the first word in the frame. A frame can contain up to 8 channels. Channels that are not included in the mask will not be sampled and stored in memory, and clocked out as '0'. In dual-phase mode, only the two LSBs are considered. For a stereo configuration, set both bits. For a mono configuration, set bit 0 only. In mono mode, only channel 0 will be sampled and stored to memory, and channel 0 will be repeated when clocked out. In mono mode, only channel 0 will be sampled and stored to memory, and channel 0 will be repeated in the second phase when clocked out. If all bits are zero, no input words will be stored to memory, and the output data lines will be constant '0'. This can be utilized when PWM debug output is desired without any actively used output pins. |
RW | 0x03 | ||
| Address Offset | 0x0000 001C | ||
| Physical Address | 0x4002 101C | Instance | 0x4002 101C |
| Description | Audio Interface PWM Debug Value | ||
| Type | RW | ||
| Bits | Field Name | Description | Type | Reset | ||
| 31:16 | RESERVED16 | Software should not rely on the value of a reserved. Writing any other value than the reset value may result in undefined behavior. | RO | 0x0000 | ||
| 15:0 | PULSE_WIDTH | The value written to this register determines the width of the active high PWM pulse (pwm_debug), which starts together with MSB of the first output word in a DMA buffer: 0x0000: Constant low 0x0001: Width of the pulse (number of BCLK cycles, here 1). ... 0xFFFE: Width of the pulse (number of BCLK cycles, here 65534). 0xFFFF: Constant high |
RW | 0x0000 | ||
| Address Offset | 0x0000 0020 | ||
| Physical Address | 0x4002 1020 | Instance | 0x4002 1020 |
| Description | DMA Input Buffer Next Pointer | ||
| Type | RW | ||
| Bits | Field Name | Description | Type | Reset | ||
| 31:0 | PTR | Pointer to the first byte in the next DMA input buffer. The read value equals the last written value until the currently used DMA input buffer is completed, and then becomes null when the last written value is transferred to the DMA controller to start on the next buffer. This event is signalized by [IRQFLAGS-AIF_DMA_IN]. At startup, the value must be written once before and once after configuring the DMA buffer size in AIFDMACFG. The next pointer must be written to this register while the DMA function uses the previously written pointer. If not written in time, IRQFLAGS.PTR_ERR will be raised and all input pins will be disabled. |
RW | 0x0000 0000 | ||
| Address Offset | 0x0000 0024 | ||
| Physical Address | 0x4002 1024 | Instance | 0x4002 1024 |
| Description | DMA Input Buffer Current Pointer | ||
| Type | RW | ||
| Bits | Field Name | Description | Type | Reset | ||
| 31:0 | PTR | Value of the DMA input buffer pointer currently used by the DMA controller. Incremented by 1 (byte) or 2 (word) for each AHB access. | RO | 0x0000 0000 | ||
| Address Offset | 0x0000 0028 | ||
| Physical Address | 0x4002 1028 | Instance | 0x4002 1028 |
| Description | DMA Output Buffer Next Pointer | ||
| Type | RW | ||
| Bits | Field Name | Description | Type | Reset | ||
| 31:0 | PTR | Pointer to the first byte in the next DMA output buffer. The read value equals the last written value until the currently used DMA output buffer is completed, and then becomes null when the last written value is transferred to the DMA controller to start on the next buffer. This event is signalized by IRQFLAGS.AIF_DMA_OUT. At startup, the value must be written once before and once after configuring the DMA buffer size in AIFDMACFG. At this time, the first two samples will be fetched from memory. The next pointer must be written to this register while the DMA function uses the previously written pointer. If not written in time, IRQFLAGS.PTR_ERR will be raised and all output pins will be disabled. |
RW | 0x0000 0000 | ||
| Address Offset | 0x0000 002C | ||
| Physical Address | 0x4002 102C | Instance | 0x4002 102C |
| Description | DMA Output Buffer Current Pointer | ||
| Type | RW | ||
| Bits | Field Name | Description | Type | Reset | ||
| 31:0 | PTR | Value of the DMA output buffer pointer currently used by the DMA controller Incremented by 1 (byte) or 2 (word) for each AHB access. | RO | 0x0000 0000 | ||
| Address Offset | 0x0000 0034 | ||
| Physical Address | 0x4002 1034 | Instance | 0x4002 1034 |
| Description | Samplestamp Generator Control Register | ||
| Type | RW | ||
| Bits | Field Name | Description | Type | Reset | ||
| 31:3 | RESERVED3 | Software should not rely on the value of a reserved. Writing any other value than the reset value may result in undefined behavior. | RO | 0b0 0000 0000 0000 0000 0000 0000 0000 | ||
| 2 | OUT_RDY | Low until the output pins are ready to be started by the samplestamp generator. When started (that is STMPOUTTRIG equals the WCLK counter) the bit goes back low. | RO | 0 | ||
| 1 | IN_RDY | Low until the input pins are ready to be started by the samplestamp generator. When started (that is STMPINTRIG equals the WCLK counter) the bit goes back low. | RO | 0 | ||
| 0 | STMP_EN | Enables the samplestamp generator. The samplestamp generator must only be enabled after it has been properly configured. When cleared, all samplestamp generator counters and capture values are cleared. |
RW | 0 | ||
| Address Offset | 0x0000 0038 | ||
| Physical Address | 0x4002 1038 | Instance | 0x4002 1038 |
| Description | Captured XOSC Counter Value, Capture Channel 0 | ||
| Type | RO | ||
| Bits | Field Name | Description | Type | Reset | ||
| 31:16 | RESERVED | Software should not rely on the value of a reserved. Writing any other value than the reset value may result in undefined behavior. | RO | 0x0000 | ||
| 15:0 | CAPT_VALUE | The value of the samplestamp XOSC counter (STMPXCNT.CURR_VALUE) last time an event was pulsed (event source selected in [EVENT.I2SSTMPSEL0.EV] for channel 0). This number corresponds to the number of 24 MHz clock cycles since the last positive edge of the selected WCLK. The value is cleared when STMPCTL.STMP_EN = 0. Note: Due to buffering and synchronization, WCLK is delayed by a small number of BCLK periods and clk periods. Note: When calculating the fractional part of the sample stamp, STMPXPER may be less than this bit field. |
RO | 0x0000 | ||
| Address Offset | 0x0000 003C | ||
| Physical Address | 0x4002 103C | Instance | 0x4002 103C |
| Description | XOSC Period Value | ||
| Type | RO | ||
| Bits | Field Name | Description | Type | Reset | ||
| 31:16 | RESERVED16 | Software should not rely on the value of a reserved. Writing any other value than the reset value may result in undefined behavior. | RO | 0x0000 | ||
| 15:0 | VALUE | The number of 24 MHz clock cycles in the previous WCLK period (that is - the next value of the XOSC counter at the positive WCLK edge, had it not been reset to 0). The value is cleared when STMPCTL.STMP_EN = 0. |
RO | 0x0000 | ||
| Address Offset | 0x0000 0040 | ||
| Physical Address | 0x4002 1040 | Instance | 0x4002 1040 |
| Description | Captured WCLK Counter Value, Capture Channel 0 | ||
| Type | RO | ||
| Bits | Field Name | Description | Type | Reset | ||
| 31:16 | RESERVED16 | Software should not rely on the value of a reserved. Writing any other value than the reset value may result in undefined behavior. | RO | 0x0000 | ||
| 15:0 | CAPT_VALUE | The value of the samplestamp WCLK counter (STMPWCNT.CURR_VALUE) last time an event was pulsed (event source selected in EVENT:I2SSTMPSEL0.EV for channel 0). This number corresponds to the number of positive WCLK edges since the samplestamp generator was enabled (not taking modification through STMPWADD/STMPWSET into account). The value is cleared when STMPCTL.STMP_EN = 0. |
RO | 0x0000 | ||
| Address Offset | 0x0000 0044 | ||
| Physical Address | 0x4002 1044 | Instance | 0x4002 1044 |
| Description | WCLK Counter Period Value | ||
| Type | RW | ||
| Bits | Field Name | Description | Type | Reset | ||
| 31:16 | RESERVED16 | Software should not rely on the value of a reserved. Writing any other value than the reset value may result in undefined behavior. | RO | 0x0000 | ||
| 15:0 | VALUE | Used to define when STMPWCNT is to be reset so number of WCLK edges are found for the size of the sample buffer. This is thus a modulo value for the WCLK counter. This number must correspond to the size of the sample buffer used by the system (that is the index of the last sample plus 1). | RW | 0x0000 | ||
| Address Offset | 0x0000 0048 | ||
| Physical Address | 0x4002 1048 | Instance | 0x4002 1048 |
| Description | WCLK Counter Trigger Value for Input Pins | ||
| Type | RW | ||
| Bits | Field Name | Description | Type | Reset | ||
| 31:16 | RESERVED16 | Software should not rely on the value of a reserved. Writing any other value than the reset value may result in undefined behavior. | RO | 0x0000 | ||
| 15:0 | IN_START_WCNT | Compare value used to start the incoming audio streams. This bit field shall equal the WCLK counter value during the WCLK period in which the first input word(s) are sampled and stored to memory (that is the sample at the start of the very first DMA input buffer). The value of this register takes effect when the following conditions are met: - One or more pins are configured as inputs in AIFDIRCFG. - AIFDMACFG has been configured for the correct buffer size, and at least 32 BCLK cycle ticks have happened. Note: To avoid false triggers, this bit field should be set higher than STMPWPER.VALUE. |
RW | 0x0000 | ||
| Address Offset | 0x0000 004C | ||
| Physical Address | 0x4002 104C | Instance | 0x4002 104C |
| Description | WCLK Counter Trigger Value for Output Pins | ||
| Type | RW | ||
| Bits | Field Name | Description | Type | Reset | ||
| 31:16 | RESERVED16 | Software should not rely on the value of a reserved. Writing any other value than the reset value may result in undefined behavior. | RO | 0x0000 | ||
| 15:0 | OUT_START_WCNT | Compare value used to start the outgoing audio streams. This bit field must equal the WCLK counter value during the WCLK period in which the first output word(s) read from memory are clocked out (that is the sample at the start of the very first DMA output buffer). The value of this register takes effect when the following conditions are met: - One or more pins are configured as outputs in AIFDIRCFG. - AIFDMACFG has been configured for the correct buffer size, and 32 BCLK cycle ticks have happened. - 2 samples have been preloaded from memory (examine the AIFOUTPTR register if necessary). Note: The memory read access is only performed when required, that is channels 0/1 must be selected in AIFWMASK0/AIFWMASK1. Note: To avoid false triggers, this bit field should be set higher than STMPWPER.VALUE. |
RW | 0x0000 | ||
| Address Offset | 0x0000 0050 | ||
| Physical Address | 0x4002 1050 | Instance | 0x4002 1050 |
| Description | WCLK Counter Set Operation | ||
| Type | RW | ||
| Bits | Field Name | Description | Type | Reset | ||
| 31:16 | RESERVED16 | Software should not rely on the value of a reserved. Writing any other value than the reset value may result in undefined behavior. | RO | 0x0000 | ||
| 15:0 | VALUE | WCLK counter modification: Sets the running WCLK counter equal to the written value. | RW | 0x0000 | ||
| Address Offset | 0x0000 0054 | ||
| Physical Address | 0x4002 1054 | Instance | 0x4002 1054 |
| Description | WCLK Counter Add Operation | ||
| Type | RW | ||
| Bits | Field Name | Description | Type | Reset | ||
| 31:16 | RESERVED16 | Software should not rely on the value of a reserved. Writing any other value than the reset value may result in undefined behavior. | RO | 0x0000 | ||
| 15:0 | VALUE_INC | WCLK counter modification: Adds the written value to the running WCLK counter. If a positive edge of WCLK occurs at the same time as the operation, this will be taken into account. To add a negative value, write "STMPWPER.VALUE - value". |
RW | 0x0000 | ||
| Address Offset | 0x0000 0058 | ||
| Physical Address | 0x4002 1058 | Instance | 0x4002 1058 |
| Description | XOSC Minimum Period Value Minimum Value of STMPXPER |
||
| Type | RW | ||
| Bits | Field Name | Description | Type | Reset | ||
| 31:16 | RESERVED16 | Software should not rely on the value of a reserved. Writing any other value than the reset value may result in undefined behavior. | RO | 0x0000 | ||
| 15:0 | VALUE | Each time STMPXPER is updated, the value is also loaded into this register, provided that the value is smaller than the current value in this register. When written, the register is reset to 0xFFFF (65535), regardless of the value written. The minimum value can be used to detect extra WCLK pulses (this registers value will be significantly smaller than STMPXPER.VALUE). |
RW | 0xFFFF | ||
| Address Offset | 0x0000 005C | ||
| Physical Address | 0x4002 105C | Instance | 0x4002 105C |
| Description | Current Value of WCNT | ||
| Type | RO | ||
| Bits | Field Name | Description | Type | Reset | ||
| 31:16 | RESERVED16 | Software should not rely on the value of a reserved. Writing any other value than the reset value may result in undefined behavior. | RO | 0x0000 | ||
| 15:0 | CURR_VALUE | Current value of the WCLK counter | RO | 0x0000 | ||
| Address Offset | 0x0000 0060 | ||
| Physical Address | 0x4002 1060 | Instance | 0x4002 1060 |
| Description | Current Value of XCNT | ||
| Type | RO | ||
| Bits | Field Name | Description | Type | Reset | ||
| 31:16 | RESERVED16 | Software should not rely on the value of a reserved. Writing any other value than the reset value may result in undefined behavior. | RO | 0x0000 | ||
| 15:0 | CURR_VALUE | Current value of the XOSC counter, latched when reading STMPWCNT. | RO | 0x0000 | ||
| Address Offset | 0x0000 0064 | ||
| Physical Address | 0x4002 1064 | Instance | 0x4002 1064 |
| Description | Internal. Only to be used through TI provided API. | ||
| Type | RO | ||
| Bits | Field Name | Description | Type | Reset | ||
| 31:16 | RESERVED16 | Internal. Only to be used through TI provided API. | RO | 0x0000 | ||
| 15:0 | CAPT_VALUE | Internal. Only to be used through TI provided API. | RO | 0x0000 | ||
| Address Offset | 0x0000 0068 | ||
| Physical Address | 0x4002 1068 | Instance | 0x4002 1068 |
| Description | Captured WCLK Counter Value, Capture Channel 1 | ||
| Type | RO | ||
| Bits | Field Name | Description | Type | Reset | ||
| 31:16 | RESERVED16 | Software should not rely on the value of a reserved. Writing any other value than the reset value may result in undefined behavior. | RO | 0x0000 | ||
| 15:0 | CAPT_VALUE | Channel 1 is idle and can not be sampled from an external event as with Channel 0 STMPWCNTCAPT0 | RO | 0x0000 | ||
| Address Offset | 0x0000 0070 | ||
| Physical Address | 0x4002 1070 | Instance | 0x4002 1070 |
| Description | Interrupt Mask Register Selects mask states of the flags in IRQFLAGS that contribute to the I2S_IRQ event. |
||
| Type | RW | ||
| Bits | Field Name | Description | Type | Reset | ||
| 31:6 | RESERVED6 | Software should not rely on the value of a reserved. Writing any other value than the reset value may result in undefined behavior. | RW | 0b00 0000 0000 0000 0000 0000 0000 | ||
| 5 | AIF_DMA_IN | IRQFLAGS.AIF_DMA_IN interrupt mask 0: Disable 1: Enable |
RW | 0 | ||
| 4 | AIF_DMA_OUT | IRQFLAGS.AIF_DMA_OUT interrupt mask 0: Disable 1: Enable |
RW | 0 | ||
| 3 | WCLK_TIMEOUT | IRQFLAGS.WCLK_TIMEOUT interrupt mask 0: Disable 1: Enable |
RW | 0 | ||
| 2 | BUS_ERR | IRQFLAGS.BUS_ERR interrupt mask 0: Disable 1: Enable |
RW | 0 | ||
| 1 | WCLK_ERR | IRQFLAGS.WCLK_ERR interrupt mask 0: Disable 1: Enable |
RW | 0 | ||
| 0 | PTR_ERR | IRQFLAGS.PTR_ERR interrupt mask. 0: Disable 1: Enable |
RW | 0 | ||
| Address Offset | 0x0000 0074 | ||
| Physical Address | 0x4002 1074 | Instance | 0x4002 1074 |
| Description | Raw Interrupt Status Register | ||
| Type | RO | ||
| Bits | Field Name | Description | Type | Reset | ||
| 31:6 | RESERVED6 | Software should not rely on the value of a reserved. Writing any other value than the reset value may result in undefined behavior. | RO | 0b00 0000 0000 0000 0000 0000 0000 | ||
| 5 | AIF_DMA_IN | Set when condition for this bit field event occurs (auto cleared when input pointer is updated - AIFINPTRNEXT), see description of AIFINPTRNEXT register for details. | RO | 0 | ||
| 4 | AIF_DMA_OUT | Set when condition for this bit field event occurs (auto cleared when output pointer is updated - AIFOUTPTRNEXT), see description of AIFOUTPTRNEXT register for details | RO | 0 | ||
| 3 | WCLK_TIMEOUT | Set when the sample stamp generator does not detect a positive WCLK edge for 65535 clk periods. This signalizes that the internal or external BCLK and WCLK generator source has been disabled. The bit is sticky and may only be cleared by software (by writing '1' to IRQCLR.WCLK_TIMEOUT). |
RO | 0 | ||
| 2 | BUS_ERR | Set when a DMA operation is not completed in time (that is audio output buffer underflow, or audio input buffer overflow). This error requires a complete restart since word synchronization has been lost. The bit is sticky and may only be cleared by software (by writing '1' to IRQCLR.BUS_ERR). Note that DMA initiated transactions to illegal addresses will not trigger an interrupt. The response to such transactions is undefined. |
RO | 0 | ||
| 1 | WCLK_ERR | Set when: - An unexpected WCLK edge occurs during the data delay period of a phase. Note unexpected WCLK edges during the word and idle periods of the phase are not detected. - In dual-phase mode, when two WCLK edges are less than 4 BCLK cycles apart. - In single-phase mode, when a WCLK pulse occurs before the last channel. This error requires a complete restart since word synchronization has been lost. The bit is sticky and may only be cleared by software (by writing '1' to IRQCLR.WCLK_ERR). |
RO | 0 | ||
| 0 | PTR_ERR | Set when AIFINPTRNEXT or AIFOUTPTRNEXT has not been loaded with the next block address in time. This error requires a complete restart since word synchronization has been lost. The bit is sticky and may only be cleared by software (by writing '1' to IRQCLR.PTR_ERR). |
RO | 0 | ||
| Address Offset | 0x0000 0078 | ||
| Physical Address | 0x4002 1078 | Instance | 0x4002 1078 |
| Description | Interrupt Set Register | ||
| Type | WO | ||
| Bits | Field Name | Description | Type | Reset | ||
| 31:6 | RESERVED6 | Software should not rely on the value of a reserved. Writing any other value than the reset value may result in undefined behavior. | WO | 0b00 0000 0000 0000 0000 0000 0000 | ||
| 5 | AIF_DMA_IN | 1: Sets the interrupt of IRQFLAGS.AIF_DMA_IN (unless a auto clear criteria was given at the same time, in which the set will be ignored) | WO | 0 | ||
| 4 | AIF_DMA_OUT | 1: Sets the interrupt of IRQFLAGS.AIF_DMA_OUT (unless a auto clear criteria was given at the same time, in which the set will be ignored) | WO | 0 | ||
| 3 | WCLK_TIMEOUT | 1: Sets the interrupt of IRQFLAGS.WCLK_TIMEOUT | WO | 0 | ||
| 2 | BUS_ERR | 1: Sets the interrupt of IRQFLAGS.BUS_ERR | WO | 0 | ||
| 1 | WCLK_ERR | 1: Sets the interrupt of IRQFLAGS.WCLK_ERR | WO | 0 | ||
| 0 | PTR_ERR | 1: Sets the interrupt of IRQFLAGS.PTR_ERR | WO | 0 | ||
| Address Offset | 0x0000 007C | ||
| Physical Address | 0x4002 107C | Instance | 0x4002 107C |
| Description | Interrupt Clear Register | ||
| Type | WO | ||
| Bits | Field Name | Description | Type | Reset | ||
| 31:6 | RESERVED6 | Software should not rely on the value of a reserved. Writing any other value than the reset value may result in undefined behavior. | WO | 0b00 0000 0000 0000 0000 0000 0000 | ||
| 5 | AIF_DMA_IN | 1: Clears the interrupt of IRQFLAGS.AIF_DMA_IN (unless a set criteria was given at the same time in which the clear will be ignored) | WO | 0 | ||
| 4 | AIF_DMA_OUT | 1: Clears the interrupt of IRQFLAGS.AIF_DMA_OUT (unless a set criteria was given at the same time in which the clear will be ignored) | WO | 0 | ||
| 3 | WCLK_TIMEOUT | 1: Clears the interrupt of IRQFLAGS.WCLK_TIMEOUT (unless a set criteria was given at the same time in which the clear will be ignored) | WO | 0 | ||
| 2 | BUS_ERR | 1: Clears the interrupt of IRQFLAGS.BUS_ERR (unless a set criteria was given at the same time in which the clear will be ignored) | WO | 0 | ||
| 1 | WCLK_ERR | 1: Clears the interrupt of IRQFLAGS.WCLK_ERR (unless a set criteria was given at the same time in which the clear will be ignored) | WO | 0 | ||
| 0 | PTR_ERR | 1: Clears the interrupt of IRQFLAGS.PTR_ERR (unless a set criteria was given at the same time in which the clear will be ignored) | WO | 0 | ||
| © 2015 - 2016. Texas Instruments | All Rights Reserved |