![]() |
![]() |
|
TI BLE5-Stack API Documentation
1.00.01.05
|
Central layer interface.
Go to the source code of this file.
Data Structures | |
| struct | gapCentralRoleCB_t |
| Central GAPRole Callback Structure. More... | |
| union | gapCentralRoleEvent_t |
| Central Event Structure. More... | |
Macros | |
| #define | GAPCENTRALROLE_BD_ADDR 0x403 |
| Device Address read from the controller (Read-only) More... | |
| #define | GAPCENTRALROLE_IRK 0x400 |
| Identity Resolving Key (Read/Write) More... | |
| #define | GAPCENTRALROLE_LINK_PARAM_UPDATE_REQ_REPLY 0x405 |
| Action taken when a parameter update fails (Read/Write) More... | |
| #define | GAPCENTRALROLE_MAX_SCAN_RES 0x404 |
| Maximmum number of scan reports to store from GAPCentralRole_StartDiscovery (Read/Write) More... | |
| #define | GAPCENTRALROLE_PARAM_UPDATE_REQ_AUTO_ACCEPT 0x01 |
| always accept what the remote peripheral is requesting. | |
| #define | GAPCENTRALROLE_PARAM_UPDATE_REQ_AUTO_REJECT 0x00 |
| always reject what the remote peripheral is requesting. | |
| #define | GAPCENTRALROLE_PARAM_UPDATE_REQ_SEND_TO_APP 0x02 |
| pass request onto application, requires a response before timeout. | |
| #define | GAPCENTRALROLE_SIGNCOUNTER 0x402 |
| Sign Counter (Read/Write) More... | |
| #define | GAPCENTRALROLE_SRK 0x401 |
| Signature Resolving Key (Read/Write) More... | |
Typedefs | |
| typedef uint8_t(* | pfnGapCentralRoleEventCB_t) (gapCentralRoleEvent_t *pEvent) |
| Central Event Callback Function. More... | |
Functions | |
| bStatus_t | GAPCentralRole_CancelDiscovery (void) |
| Cancel a device discovery scan. More... | |
| bStatus_t | GAPCentralRole_EstablishLink (uint8_t highDutyCycle, uint8_t whiteList, uint8_t addrTypePeer, uint8_t *peerAddr) |
| Establish a link to a peer device. More... | |
| bStatus_t | GAPCentralRole_GetParameter (uint16_t param, void *pValue) |
| Get a parameter in the Central Profile. More... | |
| bStatus_t | GAPCentralRole_SetParameter (uint16_t param, uint8_t len, void *pValue) |
| Set a parameter in the Central Profile. More... | |
| bStatus_t | GAPCentralRole_StartDevice (gapCentralRoleCB_t *pAppCallbacks) |
| Start the device in Central role. This function is typically called once during system startup. More... | |
| bStatus_t | GAPCentralRole_StartDiscovery (uint8_t mode, uint8_t activeScan, uint8_t whiteList) |
| Start a device discovery scan. More... | |
| bStatus_t | GAPCentralRole_TerminateLink (uint16_t connHandle) |
| Terminate a link. More... | |
| bStatus_t | GAPCentralRole_UpdateLink (uint16_t connHandle, uint16_t connIntervalMin, uint16_t connIntervalMax, uint16_t connLatency, uint16_t connTimeout) |
| Update the link connection parameters. More... | |