Go to the source code of this file.
|
| Clock_Handle | Util_constructClock (Clock_Struct *pClock, Clock_FuncPtr clockCB, uint32_t clockDuration, uint32_t clockPeriod, uint8_t startFlag, UArg arg) |
| | Initialize a TIRTOS Clock instance. More...
|
| |
| Queue_Handle | Util_constructQueue (Queue_Struct *pQueue) |
| | Initialize an RTOS queue to hold messages from profile to be processed. More...
|
| |
| char * | Util_convertBdAddr2Str (uint8_t *pAddr) |
| | Convert Bluetooth address to string. Only needed when LCD display is used. More...
|
| |
| uint8_t * | Util_dequeueMsg (Queue_Handle msgQueue) |
| | Dequeue the message from the RTOS queue. More...
|
| |
| uint8_t | Util_enqueueMsg (Queue_Handle msgQueue, Event_Handle event, uint8_t *pMsg) |
| | Creates a queue node and puts the node in RTOS queue. More...
|
| |
| bool | Util_isActive (Clock_Struct *pClock) |
| | Determine if a clock is currently active. More...
|
| |
| uint8_t | Util_isBufSet (uint8_t *pBuf, uint8_t pattern, uint16_t len) |
| | Check if contents of buffer matches byte pattern. More...
|
| |
| void | Util_rescheduleClock (Clock_Struct *pClock, uint32_t clockPeriod) |
| | Reschedule a clock by changing the timeout and period values. More...
|
| |
| void | Util_restartClock (Clock_Struct *pClock, uint32_t clockTimeout) |
| | Restart a clock by changing the timeout. More...
|
| |
| void | Util_startClock (Clock_Struct *pClock) |
| | Start a clock. More...
|
| |
| void | Util_stopClock (Clock_Struct *pClock) |
| | Stop a clock. More...
|
| |