44 #ifndef SENSOR_OPT3001_H 45 #define SENSOR_OPT3001_H bool SensorOpt3001_test(void)
Run a sensor self-test.
float SensorOpt3001_convert(uint16_t rawData)
Convert raw data to LUX.
void SensorOpt3001_enable(bool enable)
Enable/disable measurement cycle.
bool SensorOpt3001_init(void)
Initialize the temperature sensor driver.
bool SensorOpt3001_read(uint16_t *rawData)
Read the result register.