44 #ifndef SENSOR_BMP280_H 45 #define SENSOR_BMP280_H 62 #define SENSOR_BMP280_DATASIZE 6 bool SensorBmp280_read(uint8_t *pData)
Read temperature and pressure data.
bool SensorBmp280_test(void)
Run a sensor self-test.
void SensorBmp280_enable(bool enable)
Enable/disable measurement cycle.
bool SensorBmp280_init(void)
Initialize the sensor.
void SensorBmp280_convert(uint8_t *pData, int32_t *pTemp, uint32_t *pPress)
Convert raw data to object and ambiance temperature.