593 #ifndef ti_drivers_spi_SPICC26XXDMA__include 594 #define ti_drivers_spi_SPICC26XXDMA__include 607 #include <ti/drivers/dpl/HwiP.h> 608 #include <ti/drivers/dpl/SemaphoreP.h> 609 #include <ti/drivers/dpl/SwiP.h> 642 #define SPICC26XXDMA_CMD_RETURN_PARTIAL_ENABLE (SPI_CMD_RESERVED + 0) 651 #define SPICC26XXDMA_CMD_RETURN_PARTIAL_DISABLE (SPI_CMD_RESERVED + 1) 659 #define SPICC26XXDMA_CMD_SET_CSN_PIN (SPI_CMD_RESERVED + 2) 663 #define SPICC26XXDMA_RETURN_PARTIAL_ENABLE SPICC26XXDMA_CMD_RETURN_PARTIAL_ENABLE 664 #define SPICC26XXDMA_RETURN_PARTIAL_DISABLE SPICC26XXDMA_CMD_RETURN_PARTIAL_DISABLE 665 #define SPICC26XXDMA_SET_CSN_PIN SPICC26XXDMA_CMD_SET_CSN_PIN Definition: SPICC26XXDMA.h:685
uint8_t PIN_Id
Pin identifier data type.
Definition: PIN.h:550
PIN_Id csnPin
Definition: SPICC26XXDMA.h:820
const SPI_FxnTable SPICC26XXDMA_fxnTable
uint16_t defaultTxBufValue
Definition: SPICC26XXDMA.h:771
uint32_t baseAddr
Definition: SPICC26XXDMA.h:745
void(* SPI_CallbackFxn)(SPI_Handle handle, SPI_Transaction *transaction)
The definition of a callback function used by the SPI driver when used in SPI_MODE_CALLBACK.
Definition: SPI.h:561
enum SPI_Mode_ SPI_Mode
Definitions for various SPI modes of operation.
Power_NotifyObj spiPostObj
Definition: SPICC26XXDMA.h:839
unsigned int bitRate
SPI bit rate in Hz.
Definition: SPICC26XXDMA.h:806
A SPI_Transaction data structure is used with SPI_transfer(). It indicates how many SPI_FrameFormat f...
Definition: SPI.h:543
SPI_CallbackFxn transferCallbackFxn
Definition: SPICC26XXDMA.h:798
struct SPICC26XXDMA_Object * SPICC26XXDMA_Handle
uint32_t minDmaTransferSize
Definition: SPICC26XXDMA.h:786
uint8_t intPriority
SPI CC26XXDMA Peripheral's interrupt priority.
Definition: SPICC26XXDMA.h:761
uint32_t rxChannelBitMask
Definition: SPICC26XXDMA.h:773
void * spiPreFxn
Definition: SPICC26XXDMA.h:836
UDMACC26XX Global configuration.
Definition: UDMACC26XX.h:229
uint32_t txChannelBitMask
Definition: SPICC26XXDMA.h:775
uint16_t scratchBuf
Definition: SPICC26XXDMA.h:833
Power manager interface for CC26XX/CC13XX.
Power notify object structure.
Definition: Power.h:115
PIN_Id clkPin
Definition: SPICC26XXDMA.h:781
SPICC26XXDMA Hardware attributes.
Definition: SPICC26XXDMA.h:743
volatile bool spiPowerConstraint
Definition: SPICC26XXDMA.h:841
PIN_Id misoPin
Definition: SPICC26XXDMA.h:779
SPI_TransferMode transferMode
Definition: SPICC26XXDMA.h:796
SPICC26XXDMA Object.
Definition: SPICC26XXDMA.h:794
enum SPI_TransferMode_ SPI_TransferMode
SPI transfer mode determines the whether the SPI controller operates synchronously or asynchronously...
Device-specific pin & GPIO driver for CC26xx family [def].
The definition of a SPI function table that contains the required set of functions to control a speci...
Definition: SPI.h:675
void * spiPostFxn
Definition: SPICC26XXDMA.h:837
PIN_State pinState
Definition: SPICC26XXDMA.h:823
SPI_Mode mode
Definition: SPICC26XXDMA.h:799
SPICC26XXDMA_FrameSize
Definition: SPICC26XXDMA.h:684
SPICC26XXDMA_FrameSize frameSize
Definition: SPICC26XXDMA.h:817
UDMACC26XX driver implementation.
bool returnPartial
Definition: SPICC26XXDMA.h:830
struct SPICC26XXDMA_Object SPICC26XXDMA_Object
SPICC26XXDMA Object.
struct SPICC26XXDMA_HWAttrsV1 SPICC26XXDMA_HWAttrsV1
SPICC26XXDMA Hardware attributes.
PIN_Id csnPin
Definition: SPICC26XXDMA.h:783
UDMACC26XX_Handle udmaHandle
Definition: SPICC26XXDMA.h:827
uint8_t intNum
Definition: SPICC26XXDMA.h:747
PIN_Id mosiPin
Definition: SPICC26XXDMA.h:777
unsigned int transferTimeout
Definition: SPICC26XXDMA.h:797
underlying data structure for type PIN_State
Definition: PIN.h:680
enum SPI_FrameFormat_ SPI_FrameFormat
Definitions for various SPI data frame formats.
HwiP_Struct hwi
Definition: SPICC26XXDMA.h:811
SPI_FrameFormat frameFormat
Definition: SPICC26XXDMA.h:808
Power_NotifyObj spiPreObj
Definition: SPICC26XXDMA.h:838
SemaphoreP_Struct transferComplete
Definition: SPICC26XXDMA.h:813
SwiP_Struct swi
Definition: SPICC26XXDMA.h:812
bool isOpen
Definition: SPICC26XXDMA.h:843
uint32_t swiPriority
SPI SWI priority. The higher the number, the higher the priority. The minimum is 0 and the maximum is...
Definition: SPICC26XXDMA.h:767
Definition: SPICC26XXDMA.h:686
PowerCC26XX_Resource powerMngrId
Definition: SPICC26XXDMA.h:769
PIN_Handle pinHandle
Definition: SPICC26XXDMA.h:824
unsigned int dataSize
Definition: SPICC26XXDMA.h:807
SPI_Transaction * currentTransaction
Definition: SPICC26XXDMA.h:816